Hi,
We are working with a S32G-VNP-RDB2 board.
We need no flash the switch firmware to the SJA1110 flash.
According to VNPRDBEEUG document there are two ways:
- Using a PEmicro through S32DS.
- Using the provided sja1110 linux driver; this is not an option for us, since the configuration is not persistent (not written to the flash).
Could NXP provide the CMM scripts to flash the image using a T32 debug probe?
In U-Boot there is a sja1105 driver, but seems to not work with the SJA1110.
Is there any other solution?
Hi,
Within the SJA1110-EVM it is shown that a Lauterbach can be used (using the adequate probe). In the RDB2, there is a JTAG header dedicated to the SJA1110 (J44). I don't know if this is what you are looking for. Below will be a link for the SJA1110-EVM getting started guide.
Get Started with the SJA1110-EVM | NXP Semiconductors
Please, let us know if this information was helpful or not.
Hi Daniel,
Thanks for your response. Yes I already know that a T32 debug probe can be used. But I can not find the the CMM scripts for T32, and the instrucctions relates only relates to PEmicro.
Regards.
I suggest to contact Lauterbach support regarding the SJA1110. I did and they where very helpful.
Unfortunately we don't use the flash interface so I don't have the scripts you need...