Search for MCU or MPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Search for MCU or MPU

298 次查看
yangjinzhuang
Contributor III

Hello, 

       Because MPC5746r has only one Ethernet interface, so I want to find one chip ,  who has at least one lockstep core and other single core , has at least two Ethernet interfaces, and has CAN and Lin interfaces.

     S32G maybe too powerful for me, I need one chip between MPC5xxx  and S32G , which fit above requests.

     Can you give me some support?

0 项奖励
回复
1 回复

273 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For the features that you are looking, it does seem to be that S32G might be on the higher end of the spectrum. We can recommend looking into the S32K358 (or S32K388). If more information is required, since these P/Ns are still under control of distribution, we can recommend opening a ticket under the NXP online services or contacting your local NXP representative.

Also, general information can be found under the S32K3 datasheet (link: S32K3xx Data Sheet (nxp.com)). Also, we can recommend looking into the S32K community:

S32K - NXP Community

Since they should have more information that could be of use for your application.

Please, let us know.

0 项奖励
回复