Sample application to demonstrate the LLCE-PFE Can-to-Ethernet and Ethernet-to-Can bridges

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sample application to demonstrate the LLCE-PFE Can-to-Ethernet and Ethernet-to-Can bridges

1,460 Views
salimmulla2021
Contributor III

Hello, 

I have below queries with respect to the MCAL versions:

1. Is it possible to share latest stable version of the EB, LLCE, PFE and RTD?

2. is it possible to do flashing via S32 Flash tool?

Tags (1)
0 Kudos
Reply
7 Replies

1,449 Views
nxf92355
NXP Employee
NXP Employee

1. Is it possible to share latest stable version of the EB, LLCE, PFE and RTD?

-> you need software account for same.

2. is it possible to do flashing via S32 Flash tool?

-> yes , you can flash

Tags (1)
0 Kudos
Reply

1,444 Views
salimmulla2021
Contributor III

Hello,

I have NXP account and everything. So, request you to provide details of the version information and steps for flashing without debugger. 

 

0 Kudos
Reply

1,429 Views
nxf92355
NXP Employee
NXP Employee
If you have software account , then you can directly see version information for same.
got to as below image and click on Software account >  view account
 
Screenshot from 2023-05-03 12-16-37.png

 

Regards ,
Tushar
0 Kudos
Reply

1,400 Views
nxf92355
NXP Employee
NXP Employee

did got version and s32G flash tools pdf ?

0 Kudos
Reply

1,394 Views
salimmulla2021
Contributor III

I got the PDF but Could you please let me know how to convert the generated elf file to bin file and what are the placements of IVT image or is that possible to flash elf file?  As per below ticket there is no S2DS project for PFE.

Re: CAN2ETH and ETH2CAN LLCE example for S32DS - NXP Community

 

0 Kudos
Reply

1,387 Views
nxf92355
NXP Employee
NXP Employee

Hi Salim Mulla

To generate .bin file , Read S32G-VNP-RDB2 SOFTWARE ENABLEMENT GUIDE. Read from page number 19 which describes steps to generate .bin file . IVT setup also describes. I attached that guide please refer it.

Thanks & Regards,

Tushar

0 Kudos
Reply

1,440 Views
nxf92355
NXP Employee
NXP Employee

Hi Salim Mulla

Please read S32_Flash_Tool_User_Guide.pdf. it available at location  NXP/S32DS.3.4/S32DS/tools/S32FlashTool/doc/

Thanks & Regards,

Tushar

0 Kudos
Reply