SD on S32g rdb2 cannot generate insertion and remove interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD on S32g rdb2 cannot generate insertion and remove interrupt

Jump to solution
2,683 Views
HangSong
Contributor II

Hi @nxp,

Can't S32G RDB2 perform SD card plug-in detection through CD?

I am doing SD card support on S32G RDB2.
IRQSTATEN and IRQSIGEN write 0x17f00c3, enabling CINSSEN and CRMSEN.
When the SD card is pulled out and inserted, there will be no corresponding interrupt, and the register PRSSTAT[CINST], INT_STATUS[CINS] and INT_STATUS[CRM] will not change.

Thanks,
Song

Tags (2)
0 Kudos
Reply
1 Solution
2,648 Views
bpe
NXP Employee
NXP Employee

uSDHC SD Card detect signals are not routed outside S32G2, this function is not
available on it.

Best Regards,
Platon

 

View solution in original post

0 Kudos
Reply
2 Replies
2,649 Views
bpe
NXP Employee
NXP Employee

uSDHC SD Card detect signals are not routed outside S32G2, this function is not
available on it.

Best Regards,
Platon

 

0 Kudos
Reply
2,634 Views
HangSong
Contributor II

Hi @bpe ,

Got it. Thank you.

Best Regards,
Song

 

0 Kudos
Reply