S32G Uboot tftp download files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G Uboot tftp download files

ソリューションへジャンプ
999件の閲覧回数
learnx
Contributor III

Referring to the AN13185 document, files can be downloaded normally using GMAC. Now I want to use other interfaces, such as PFE MAC1. How should I configure Uboot’s environment variables?

learnx_0-1711424531162.png

 

0 件の賞賛
返信
1 解決策
974件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @learnx

I just created BSP33 images and use them running on a RDB2 to have a try locally.

I found that with the following settings from uboot variables based on default settings, the PFE2(U58 from the picture you attached) could be used under u-boot to communicate with the host:

setenv pfengemac 2

setenv ipaddr xxxx

setenv serverip xxxx

ping $serverip

Attached to pfe2

Using eth_pfeng device

host xxxxx is alive

 

Hope it helps.

 

Best Regards

Chenyin

元の投稿で解決策を見る

6 返答(返信)
975件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @learnx

I just created BSP33 images and use them running on a RDB2 to have a try locally.

I found that with the following settings from uboot variables based on default settings, the PFE2(U58 from the picture you attached) could be used under u-boot to communicate with the host:

setenv pfengemac 2

setenv ipaddr xxxx

setenv serverip xxxx

ping $serverip

Attached to pfe2

Using eth_pfeng device

host xxxxx is alive

 

Hope it helps.

 

Best Regards

Chenyin

811件の閲覧回数
Fuan_Ning
Contributor I

您好!

请问s32g2ardb2在uboot阶段是否可以ping通pfe_emac0,也就是通过连接sja1110网口使用tftp,如何操作

谢谢

0 件の賞賛
返信
809件の閲覧回数
Fuan_Ning
Contributor I
s32g274ardb2
bsp33
0 件の賞賛
返信
971件の閲覧回数
learnx
Contributor III

thank you

0 件の賞賛
返信
983件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @learnx

Thanks for the questions

I could understand that you are using a RDB2, may I know which BSP used in your test? You may want to download images under U-boot via PFE port, is it right?

 

Best Regards

Chenyin

0 件の賞賛
返信
981件の閲覧回数
learnx
Contributor III

Sorry, the background of my question and my requirements are not very clear. I will ask again.
Hardware environment: S32G274ARDB2
Software environment: BSP33.0
Requirement: Download the sdcard image through the PFE port in Uboot
What I tried:
1. Follow the steps described in 2.3.4 "Flashing image with SD card-less" of document AN13185 to download the image normally. The port used in the document is GMAC.
2. I want to download the image through the PFE port. Under uboot, I tried to modify the environment variables ethact, pfengmac, pfeng_mode, ipaddr and serverip, but none of them successfully communicated with my host.

0 件の賞賛
返信