S32G IPCF runs in an endless loop

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G IPCF runs in an endless loop

857件の閲覧回数
jack_huang1
Contributor III

Dear,

The S32G2 platform is based on IPCF4.8.0.

Q1:  After the configuration is interrupted 19, the program keeps entering the ISR(Ipc_Hard_irq_handle) function after running. See Appendix 1 for the implementation of the function.       

Q2: IPCF reverted to version 4.6.0 with an unhandleirq error, and then IPCF changed from 4.6.0 to 4.8.0 with the same error screenshot as attached 2.

 Thank you!

 Best Regards!

0 件の賞賛
返信
2 返答(返信)

840件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi Jack

 

Hope you are doing well

Can you some brief on "After the configuration is interrupted 19" ?

Can you tell which document you are talking "Appendix 1 for the implementation of the function" ?

 

Regards ,

Tushar

 

0 件の賞賛
返信

800件の閲覧回数
jack_huang1
Contributor III

Dear Tushar:

          It's solved now, because our system versions don't match it.

 

         Thank you!

          Best Regards!

0 件の賞賛
返信