S32G Goldvip CAN usecase hardware setup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32G Goldvip CAN usecase hardware setup

577 次查看
Vishnu13
Contributor I

Hi,

I want to test the CAN usecase.

I connected the following pins using wires:

i) FlexCAN0(L) to LLCE-CAN0 (L)

ii) FlexCAN0(H) to LLCE-CAN0 (H)

iii) FlexCAN1(L) to LLCE-CAN1(L)

iv) FlexCAN1(H) to LLCE-CAN1(H)

 

I executed the following script:

./canperf.sh -t can0 -r can1 -i 0 -o 4 -s 64 -g 0 -l 10

 

But the output was not as expected. Attaching the generated report below.

1665062477469(1).jpg

Could you please explain what could be the issue here? Is there any additional hardware requirement? The image used is golvip1.3.0

0 项奖励
回复
1 回复

571 次查看
gmocanu
NXP Employee
NXP Employee

Hello, Vishnu,

 

The fact that the reported M7 core loads are 0% tells me that the application doesn't run at all. Are you sure you booted from QSPI? The SW4.7 DIP switch should be set to OFF.

 

Best regards,

George

0 项奖励
回复