RMII & Fixed-link under PFE TX OK but RX NG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RMII & Fixed-link under PFE TX OK but RX NG

Jump to solution
7,264 Views
StanleyShen
Contributor IV

Hi there,

We want to connect  a 5G modules call by AG551 through RMII under PFE like blow image,

 ping AG551 from S32G274A , the ARP packet send to AG551 is OK(tcpdump shows), but the ARP answer, but the response cannot be returned from AG551 to S32G274A.

StanleyShen_3-1692784131821.png

here are our dts

S32G274A

diff --git a/arch/arm64/boot/dts/freescale/s32gxxxa-rdb.dtsi b/arch/arm64/boot/dts/freescale/s32gxxxa-rdb.dtsi
index e1fbd28bb..f5c585bd4 100644
--- a/arch/arm64/boot/dts/freescale/s32gxxxa-rdb.dtsi
+++ b/arch/arm64/boot/dts/freescale/s32gxxxa-rdb.dtsi
@@ -72,8 +72,11 @@
 };
 
 &pfe_netif2 {
-       phy-mode = "rgmii-id";
-       phy-handle = <&pfe_mdio_b_phy4>;
+       phy-mode = "rgmii";
+       fixed-link {
+               speed = <1000>;
+               full-duplex;
+       };
 };

 

AG551

        ethqos_hw: qcom,ethernet@00020000 {
                compatible = "qcom,sdxprairie-ethqos";
                qcom,arm-smmu;
                //emac-phy-addr = <7>;    //Mars.Chen 20210624  find external PHY addr by scan 0 to 31,not set by dtsi
                reg = <0x20000 0x10000>,
                        <0x36000 0x100>,
                        <0xf100000 0x300000>;
                reg-names = "stmmaceth", "rgmii","tlmm-central-base";
                clocks = <&clock_gcc GCC_ETH_AXI_CLK>,
                        <&clock_gcc GCC_ETH_SLAVE_AHB_CLK>,
                        <&clock_gcc GCC_ETH_PTP_CLK>,
                        <&clock_gcc GCC_ETH_RGMII_CLK>;
                clock-names = "stmmaceth", "pclk", "ptp_ref", "rgmii";
                snps,ptp-ref-clk-rate = <230400000>;
                snps,ptp-req-clk-rate = <57600000>;
                //interrupts-extended = <&pdc 0 62 4>, <&pdc 0 60 4>,
                interrupts-extended = <&pdc 0 62 4>,                         //Mars.chen 2021-06-15
                        <&tlmm 90 2>, <&pdc 0 290 1>, <&pdc 0 291 1>;
                //interrupt-names = "macirq", "eth_lpi",
                interrupt-names = "macirq",                                  //Mars.chen 2021-06-15,repair eth_lpi irq storm cause sytstem dump
                        "phy-intr",     "ptp_pps_irq_0", "ptp_pps_irq_1";    //eth_lpi irq only about PHY IEEE function,now not use it
                snps,crc_strip;
                qcom,msm-bus,name = "emac";
                qcom,msm-bus,num-cases = <5>;
                qcom,msm-bus,num-paths = <2>;
                qcom,msm-bus,vectors-KBps =
                        <98 512 0 0>, <1 781 0 0>,  /* No vote */
                        <98 512 2500 0>, <1 781 0 40000>,  /* 10Mbps vote */
                        <98 512 25000 0>, <1 781 0 40000>,  /* 100Mbps vote */
                        <98 512 250000 0>, <1 781 0 40000>, /* 1000Mbps vote */
                        <98 512 250000 0>, <1 781 0 400000>; /* Nominal vote */
                qcom,bus-vector-names = "0", "10", "100", "1000", "Nominal";                                                                                                           
                snps,tso;
                snps,pbl = <32>;
                mac-address = [00 55 7B B5 7D f7];
                rx-fifo-depth = <16384>;
                tx-fifo-depth = <20480>;
                snps,mtl-rx-config = <&mtl_rx_setup>;
                snps,mtl-tx-config = <&mtl_tx_setup>;

                vreg_rgmii-supply = <&pmxprairie_vref_rgmii>;
                vreg_emac_phy-supply =  <&vreg_emac_phy>;
                vreg_rgmii_io_pads-supply = <&vreg_rgmii_io_pads>;
                gdsc_emac-supply = <&gdsc_emac>;

                qcom,phy-intr-redirect = <&tlmm 90 GPIO_ACTIVE_LOW>;
                //Mars 2020/11/23,PPS-0 & PPS-1 not use,release gpio106 & gpio95
                //pinctrl-names = "dev-emac_pin_pps_0", "dev-emac_pin_pps_1";
                //pinctrl-0 = <&emac_pin_pps_0>;
                //pinctrl-1 = <&emac_pin_pps_1>;

                //Mars.chen 2022-05-24,if customer want AG55x control PHY power,can configure by [quec,phy-pwren-gpio]
                //quec,phy-pwren-gpio = <&tlmm 102 GPIO_ACTIVE_HIGH>;
                snps,reset-gpio = <&tlmm 91 GPIO_ACTIVE_LOW>;

                snps,reset-active-low;
                snps,reset-delays-us = <0 11000 70000>;
                phy-mode = "rgmii";

                ethqos_emb_smmu: ethqos_emb_smmu {
                        compatible = "qcom,emac-smmu-embedded";
                        iommus = <&apps_smmu 0x1c0 0xf>;
                        qcom,iova-mapping = <0x80000000 0x0FE40000>;
                        qcom,smmu-fastmap;
                        qcom,smmu-geometry;
                };
                io-macro-info {
                        prg-rclk-dly = <1500>;
                };
        };
...
&ethqos_hw {
        /delete-property/ vreg_rgmii-supply;
//Mars 2020/11/23,PPS-0 & PPS-1 not use,release gpio106 & gpio95
//      pinctrl-names = "default",
//              "dev-emac_pin_pps_0",
//              "dev-emac_pin_pps_1";
        pinctrl-0 = <&vreg_rgmii_off_default>; //Mars.chen 2021-06-18,change for vddio support 1.8v
//      pinctrl-1 = <&emac_pin_pps_0>;
//      pinctrl-2 = <&emac_pin_pps_1>;
        qcom,phy-reset-delay-msecs = <10>;
        ipa-dma-rx-desc-cnt = <512>;
        ipa-dma-tx-desc-cnt = <512>;
        rgmii-tx-drv-str-clk = <16>;
        rgmii-tx-drv-str-data = <16>;
        rgmii-tx-drv-str-ctl = <16>;
};

 

Could you tell us the reason and how to fix it?

Thank you

 

0 Kudos
Reply
1 Solution
6,997 Views
MayanksPatel
NXP Employee
NXP Employee

Hi @StanleyShen,

Thank you for your patience.

The root cause of this issue is PFE MAC2 RX clock from the 5G module is not ready While initializing the PFE-related clock, the PFE_MAC2 RX clock is out of lock.

Temp workaround:

Load the PFE Linux driver after the 5G module is functional(Wait for the RX clock from the 5G module to be stable).

 

Hope this helps.

 

Thanks,

Mayank S Patel

 
 

View solution in original post

0 Kudos
Reply
11 Replies
7,071 Views
StanleyShen
Contributor IV

Can somebody help me?

0 Kudos
Reply
7,145 Views
StanleyShen
Contributor IV

Dear @MayanksPatel 

Today, we have analysed the GRMII logic by saleae tool, 

It seem that the nxp receive NG, could you tell us the reason?

StanleyShen_0-1693213796090.png

 

StanleyShen_1-1693213817520.png

 

 

 

0 Kudos
Reply
7,215 Views
StanleyShen
Contributor IV

Also, since the Quectel FAE told us that we can adjust the RGMII delay time, could you tell me how to change it, thank you.

0 Kudos
Reply
7,206 Views
MayanksPatel
NXP Employee
NXP Employee

Hi @StanleyShen,

Can you please elaborate more on the RGMII Delay Time? What delay do you need to change?

 Also, have you checked that the Quectel module is connected and IP assigned to it?

 

 

Thanks,

Mayank S Patel

0 Kudos
Reply
7,180 Views
StanleyShen
Contributor IV

Dear @MayanksPatel 

Can you please elaborate more on the RGMII Delay Time? What delay do you need to change?

I want to change Delay Tiem to 2ns, but at present, I don't know if modifying the delay time can solve my problem, and whether to modify the delay time of RGMII or PFE.

 Also, have you checked that the Quectel module is connected and IP assigned to it?

Yes, I manually set the IP of AG55 to 192.168.1.100:

===================== Ping from S32G274A to Quectel ====================

Quectel module side:

StanleyShen_0-1692971296220.png

S32G274A side:

StanleyShen_4-1692971543722.png

 

StanleyShen_1-1692971316739.png

===================== Ping from Quectel to S32G274A  ====================

S32G274A side:

StanleyShen_2-1692971468640.png

StanleyShen_6-1692971618990.png

 

Quectel module side:

StanleyShen_3-1692971479249.png

StanleyShen_5-1692971598908.png

 

0 Kudos
Reply
7,037 Views
MayanksPatel
NXP Employee
NXP Employee

Hi @StanleyShen,

I have created a ticket with the internal team. I will get back to you on this.

Thank you for your patience.

 

Thanks,

Mayank S Patel

0 Kudos
Reply
7,239 Views
StanleyShen
Contributor IV

S32G Log

StanleyShen_2-1692803497503.png

 

root@s32g274ardb2:~# ping 192.168.100.100
PING 192.168.100.100 (192.168.100.100) 56(84) bytes of data.
From 192.168.100.101 icmp_seq=1 Destination Host Unreachable
From 192.168.100.101 icmp_seq=2 Destination Host Unreachable
From 192.168.100.101 icmp_seq=3 Destination Host Unreachable
^C
--- 192.168.100.100 ping statistics ---
6 packets transmitted, 0 received, +3 errors, 100% packet loss, time 5104ms

AG55 capture log

StanleyShen_1-1692803386571.png

StanleyShen_0-1692803659731.png

 

 

StanleyShen_0-1692799673296.png

 

0 Kudos
Reply
6,998 Views
MayanksPatel
NXP Employee
NXP Employee

Hi @StanleyShen,

Thank you for your patience.

The root cause of this issue is PFE MAC2 RX clock from the 5G module is not ready While initializing the PFE-related clock, the PFE_MAC2 RX clock is out of lock.

Temp workaround:

Load the PFE Linux driver after the 5G module is functional(Wait for the RX clock from the 5G module to be stable).

 

Hope this helps.

 

Thanks,

Mayank S Patel

 
 
0 Kudos
Reply
6,923 Views
StanleyShen
Contributor IV

Hi @MayanksPatel 

Thank you for you replay.

Previously, we also found this situation and resolved it using the same method.

Thank you again

 

0 Kudos
Reply
6,940 Views
yanglei666888
Contributor II

The PFE of my board is connected to the sja1105 switch. The device tree of Linux DSA  driver requires the cpu port to be configured, so the PFE must be initialized first. the PFE_MAC RX clock is out of lock .How do I configure it correctly?

&spi1 {
spi-num-chipselects = <1>;
#address-cells = <1>;
#size-cells = <0>;
status = "okay";

sja1105q_A@0 {
compatible = "nxp,sja1105q";
spi-max-frequency = <0x3D0900>;
spi-cpha;
fsl,spi-cs-sck-delay = <1>;
fsl,spi-sck-cs-delay = <1>;

reg = <0>;
soft-cs-gpio = <&pcal6524B 17 0>;
reset-gpio = <&pcal6524B 16 0>;
dsa,member = < 0 0 >;

ports {
#address-cells = <1>;
#size-cells = <0>;
switchAp0: port@0 {
ethernet = <&pfe_netif1>;
phy-mode = "rgmii-id";
label = "cpu";
reg = <0>;
fixed-link {
speed = <1000>;
full-duplex;
};
};

switchAp1:port@1 {
phy-handle = <&mdio_a_phy_A1>;
phy-mode = "rgmii-id";
label = "Sw_A_p1";
reg = <1>;
};

switchAp2: port@2 {
phy-handle = <&mdio_a_phy_A2>;
phy-mode = "rgmii-id";
label = "Sw_A_p2";
reg = <2>;
};

switchAp3: port@3 {
phy-handle = <&mdio_a_phy_A3>;
phy-mode = "rgmii-id";
label = "Sw_A_p3";
reg = <3>;
};

switchAp4: port@4 {
phy-mode = "rgmii";
label = "Sw_A_p4";
reg = <4>;
fixed-link {
speed = <1000>;
full-duplex;
};
};
};
};
};

0 Kudos
Reply
6,886 Views
MayanksPatel
NXP Employee
NXP Employee

Hi @yanglei666888,

Please raise a new ticket for the queries.

 

 

Thanks,

Mayank S Patel

0 Kudos
Reply