PFE0 not working with BSP34

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PFE0 not working with BSP34

8,850 次查看
yellapu_anishkh
Contributor IV

Hi Team,

Test Boards: RDB3, Custom board.

Software BSP: BSP34

BSP34 Linux BSP user manual was missing from NXP portal. Could you please share the same, as we are the reference command from BSP33.

One BSP33, PFE0 is configured to SGMII and we are able to ping the device.

The same SERDES1 configuration when tried with BSP34, at uboot the configuration is not taken and in Linux ping is not working.

Below are the command tried on BSP34 from u-boot.

command :

hwconfig=pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=2G5

In uboot it didnt showed the SERDES1 configuration and ping didnt worked on pfe0, even there is no error from pfe driver log.

/***********************************Log**********************************/

NOTICE: Reset status: Power-On Reset
NOTICE: BL2: v2.5(release):bsp34.0.1-2.5
NOTICE: BL2: Built : 07:11:12, Sep 6 2022
NOTICE: BL2: Booting BL31


U-Boot 2020.04+g6391b468b1 (Sep 12 2022 - 14:11:05 +0000)

CPU: NXP S32G399A rev. 1.0
Model: NXP S32G399A-RDB3
DRAM: 3.5 GiB
MMC: FSL_SDHC: 0
Loading Environment from MMC... OK
Configuring PCIe0 as RootComplex
Setting PCI Device and Vendor IDs to 0x4300:0x1957
PCIe0: Failed to get link up
Pcie0: LINK_DBG_1: 0x00000000, LINK_DBG_2: 0x00000800 (expected 0x000000d1)
DEBUG_R0: 0x0077c700, DEBUG_R1: 0x08200000
PCI: Failed autoconfig bar 1c
In: serial@401c8000
Out: serial@401c8000
Err: serial@401c8000
Board revision: RDB3
Net: EQOS phy: rgmii @ 1

Warning: eth_eqos (eth0) using random MAC address - 9a:f8:8d:cb:e1:85
eth0: eth_eqosFailed to get speed of XPCS for emac1_xpcs PFE: emac0: sgmii emac1: sgmii emac2: rgmii

Warning: eth_pfeng using MAC address from ROM
, eth1: eth_pfeng
Hit any key to stop autoboot: 0
=> printenv hwconfig
hwconfig=pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=2G5
=> reset
resetting þNOTICE: Reset status: Destructive Reset (RUN)
NOTICE: BL2: v2.5(release):bsp34.0.1-2.5
NOTICE: BL2: Built : 07:11:12, Sep 6 2022
NOTICE: BL2: Booting BL31


U-Boot 2020.04+g6391b468b1 (Sep 12 2022 - 14:11:05 +0000)

CPU: NXP S32G399A rev. 1.0
Model: NXP S32G399A-RDB3
DRAM: 3.5 GiB
MMC: FSL_SDHC: 0
Loading Environment from MMC... OK
Configuring PCIe0 as RootComplex
Setting PCI Device and Vendor IDs to 0x4300:0x1957
PCIe0: Failed to get link up
Pcie0: LINK_DBG_1: 0x00000000, LINK_DBG_2: 0x00000800 (expected 0x000000d1)
DEBUG_R0: 0x007d1700, DEBUG_R1: 0x08200000
PCI: Failed autoconfig bar 1c
In: serial@401c8000
Out: serial@401c8000
Err: serial@401c8000
Board revision: RDB3
Net: EQOS phy: rgmii @ 1

Warning: eth_eqos (eth0) using random MAC address - ba:be:a0:c2:6c:2b
eth0: eth_eqosFailed to get speed of XPCS for emac1_xpcs PFE: emac0: sgmii emac1: sgmii emac2: rgmii

Warning: eth_pfeng using MAC address from ROM
, eth1: eth_pfeng
Hit any key to stop autoboot: 0
=> boot
PFE: emac0: sgmii emac1: sgmii emac2: rgmii
PFE: emac0: sgmii emac1: sgmii emac2: rgmii
switch to partitions #0, OK
mmc0 is current device
13756424 bytes read in 599 ms (21.9 MiB/s)
Booting from mmc ...
45919 bytes read in 16 ms (2.7 MiB/s)
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 0000000083000000, end 000000008300e35e
fixup: pfe0 set to 00:01:be:be:ef:11
fixup: pfe1 set to 00:01:be:be:ef:22
fixup: pfe1: update phy addr to 0x8
fixup: pfe2 set to 00:01:be:be:ef:33

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.10.120-rt70+g0b76731696c1 (oe-user@oe-host) (aarch64-fsl-linux-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.35.1) #1 SMP PREEMPT Mon Sep 12 13:23:16 UTC 2022
[ 0.000000] Machine model: NXP S32G399A-RDB3
[ 0.000000] earlycon: linflex0 at MMIO 0x00000000401c8000 (options '115200n8')
[ 0.000000] printk: bootconsole [linflex0] enabled
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000083200000, size 3 MiB
[ 0.000000] OF: reserved mem: initialized node pfebufs@83200000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x00000008dfffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000831fffff]
[ 0.000000] node 0: [mem 0x0000000083200000-0x00000000835dffff]
[ 0.000000] node 0: [mem 0x00000000835e0000-0x0000000083ffffff]
[ 0.000000] node 0: [mem 0x0000000084000000-0x000000008407ffff]
[ 0.000000] node 0: [mem 0x0000000084080000-0x00000000bfffffff]
[ 0.000000] node 0: [mem 0x00000000c0000000-0x00000000c07fffff]
[ 0.000000] node 0: [mem 0x00000000c0800000-0x00000000cfffffff]
[ 0.000000] node 0: [mem 0x00000000d0000000-0x00000000d03fffff]
[ 0.000000] node 0: [mem 0x00000000d0400000-0x00000000ffffffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000008dfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008dfffffff]
[ 0.000000] On node 0 totalpages: 917504
[ 0.000000] DMA zone: 7168 pages used for memmap
[ 0.000000] DMA zone: 0 pages reserved
[ 0.000000] DMA zone: 524288 pages, LIFO batch:63
[ 0.000000] Normal zone: 5376 pages used for memmap
[ 0.000000] Normal zone: 393216 pages, LIFO batch:63
[ 0.000000] cma: Reserved 256 MiB at 0x00000000ef800000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 17 pages/cpu s30936 r8192 d30504 u69632
[ 0.000000] pcpu-alloc: s30936 r8192 d30504 u69632 alloc=17*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3 [0] 4 [0] 5 [0] 6 [0] 7
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, 1530923, or 1530924
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 904960
[ 0.000000] Kernel command line: console=ttyLF0,115200 root=/dev/mmcblk0p2 rootwait rw earlycon nohz=off coherent_pool=64M
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0x00000000eb800000-0x00000000ef800000] (64MB)
[ 0.000000] Memory: 3237836K/3670016K available (8574K kernel code, 634K rwdata, 2816K rodata, 1344K init, 238K bss, 170036K reserved, 262144K cma-reserved)
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: 544 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: MBI range [167:182]
[ 0.000000] GICv3: Using MBI frame 0x0000000050800000
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000050900000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] arch_timer: cp15 timer(s) running at 5.00MHz (virt).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x127350b88, max_idle_ns: 440795202120 ns
[ 0.000001] sched_clock: 56 bits at 5MHz, resolution 200ns, wraps every 4398046511100ns
[ 0.008512] Console: colour dummy device 80x25
[ 0.012543] Calibrating delay loop (skipped), value calculated using timer frequency.. 10.00 BogoMIPS (lpj=20000)
[ 0.022764] pid_max: default: 32768 minimum: 301
[ 0.027506] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.034754] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.043967] rcu: Hierarchical SRCU implementation.
[ 0.048896] smp: Bringing up secondary CPUs ...
[ 0.053503] Detected VIPT I-cache on CPU1
[ 0.057101] GICv3: CPU1: found redistributor 1 region 0:0x0000000050920000
[ 0.063956] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.070980] Detected VIPT I-cache on CPU2
[ 0.074574] GICv3: CPU2: found redistributor 100 region 0:0x0000000050980000
[ 0.081613] CPU2: Booted secondary processor 0x0000000100 [0x410fd034]
[ 0.088631] Detected VIPT I-cache on CPU3
[ 0.092211] GICv3: CPU3: found redistributor 101 region 0:0x00000000509a0000
[ 0.099247] CPU3: Booted secondary processor 0x0000000101 [0x410fd034]
[ 0.106264] Detected VIPT I-cache on CPU4
[ 0.109847] GICv3: CPU4: found redistributor 2 region 0:0x0000000050940000
[ 0.116713] CPU4: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.123706] Detected VIPT I-cache on CPU5
[ 0.127287] GICv3: CPU5: found redistributor 3 region 0:0x0000000050960000
[ 0.134147] CPU5: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.141140] Detected VIPT I-cache on CPU6
[ 0.144721] GICv3: CPU6: found redistributor 102 region 0:0x00000000509c0000
[ 0.151761] CPU6: Booted secondary processor 0x0000000102 [0x410fd034]
[ 0.158764] Detected VIPT I-cache on CPU7
[ 0.162346] GICv3: CPU7: found redistributor 103 region 0:0x00000000509e0000
[ 0.169381] CPU7: Booted secondary processor 0x0000000103 [0x410fd034]
[ 0.175962] smp: Brought up 1 node, 8 CPUs
[ 0.179969] SMP: Total of 8 processors activated.
[ 0.184648] CPU features: detected: 32-bit EL0 Support
[ 0.189780] CPU features: detected: CRC32 instructions
[ 0.202156] CPU: All CPU(s) started at EL1
[ 0.205849] alternatives: patching kernel code
[ 0.210897] devtmpfs: initialized
[ 0.219610] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.228930] futex hash table entries: 2048 (order: 5, 131072 bytes, linear)
[ 0.242500] pinctrl core: initialized pinctrl subsystem
[ 0.248086] NET: Registered protocol family 16
[ 0.253554] DMA: preallocated 4096 KiB GFP_KERNEL pool for atomic allocations
[ 0.261172] DMA: preallocated 4096 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.269480] DMA: preallocated 4096 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.277380] thermal_sys: Registered thermal governor 'step_wise'
[ 0.277691] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.290154] ASID allocator initialised with 65536 entries
[ 0.295481] Serial: AMBA PL011 UART driver
[ 0.300070] arm-scmi firmware:scmi: SCMI Notifications - Core Enabled.
[ 0.306205] arm-scmi firmware:scmi: No. of Protocol > MAX_PROTOCOLS_IMP
[ 0.312757] arm-scmi firmware:scmi: SCMI Protocol v2.0 'NXP:S32G399A' Firmware version 0x0
[ 0.341384] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.347656] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.354342] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.361030] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.370951] scmi-clocks scmi_dev.1: failed to register clock 87
[ 0.376449] scmi-clocks scmi_dev.1: failed to register clock 88
[ 0.382346] scmi-clocks scmi_dev.1: failed to register clock 89
[ 0.388244] scmi-clocks scmi_dev.1: failed to register clock 90
[ 0.394212] scmi-clocks scmi_dev.1: failed to register clock 95
[ 0.400048] scmi-clocks scmi_dev.1: failed to register clock 96
[ 0.405953] scmi-clocks scmi_dev.1: failed to register clock 97
[ 0.411852] scmi-clocks scmi_dev.1: failed to register clock 98
[ 0.421076] vgaarb: loaded
[ 0.423500] SCSI subsystem initialized
[ 0.427202] usbcore: registered new interface driver usbfs
[ 0.432573] usbcore: registered new interface driver hub
[ 0.437863] usbcore: registered new device driver usb
[ 0.443232] pps_core: LinuxPPS API ver. 1 registered
[ 0.447822] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.456947] PTP clock support registered
[ 0.461540] clocksource: Switched to clocksource arch_sys_counter
[ 0.471986] NET: Registered protocol family 2
[ 0.476086] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.484808] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 0.492943] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.500990] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[ 0.508613] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.514809] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.521454] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.528696] NET: Registered protocol family 1
[ 0.533272] RPC: Registered named UNIX socket transport module.
[ 0.538759] RPC: Registered udp transport module.
[ 0.543445] RPC: Registered tcp transport module.
[ 0.548138] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.554574] PCI: CLS 0 bytes, default 64
[ 0.559191] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.567694] workingset: timestamp_bits=62 max_order=20 bucket_order=0
[ 0.574428] fuse: init (API version 7.32)
[ 0.578118] NET: Registered protocol family 38
[ 0.582451] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
[ 0.589807] io scheduler mq-deadline registered
[ 0.594318] io scheduler kyber registered
[ 0.599640] s32g-siul2-pinctrl 4009c240.siul2-pinctrl: initialized s32 pinctrl driver
[ 0.607966] gpio-345 (sja1110-rst-phy-t1): hogged as output/low
[ 0.613464] gpio-402 (sja1110-rst-core): hogged as output/low
[ 0.621114] serial: Freescale linflex driver
[ 0.634743] printk: console [ttyLF0] enabled0x401c8000 (irq = 34, base_baud = 7812500) is a FSL_LINFLEX
[ 0.634743] printk: console [ttyLF0] enabled
[ 0.643441] printk: bootconsole [linflex0] disabled
[ 0.643441] printk: bootconsole [linflex0] disabled
[ 0.653743] 401cc000.serial: ttyLF1 at MMIO 0x401cc000 (irq = 35, base_baud = 7812500) is a FSL_LINFLEX
[ 0.663661] 402bc000.serial: ttyLF2 at MMIO 0x402bc000 (irq = 56, base_baud = 7812500) is a FSL_LINFLEX
[ 0.674733] fsl_fccu 4030c000.fccu: FCCU status is 0 (normal)
[ 0.683851] spi-nor spi6.0: mx25uw51245g (65536 Kbytes)
[ 0.689616] 7 fixed-partitions partitions found on MTD device 0.spi
[ 0.696011] Creating 7 MTD partitions on "0.spi":
[ 0.700814] 0x000000000000-0x000004000000 : "Flash-Image"
[ 0.706558] 0x000000000000-0x0000001e0000 : "FIP"
[ 0.711550] 0x0000001e0000-0x0000001f0000 : "U-Boot-Env"
[ 0.717171] 0x0000001f0000-0x000000ff0000 : "Kernel"
[ 0.722439] 0x000000ff0000-0x0000010f0000 : "DTB"
[ 0.727431] 0x0000010f0000-0x000003000000 : "Rootfs"
[ 0.732695] 0x000003000000-0x000004000000 : "PFE-Firmware"
[ 0.739558] vcan: Virtual CAN interface driver
[ 0.744094] slcan: serial line CAN interface driver
[ 0.749067] slcan: 10 dynamic interface channels.
[ 0.753864] CAN device driver interface
[ 0.758450] flexcan 401b4000.flexcan: device registered (reg_base=(____ptrval____), irq(s):
[ 0.766973] flexcan 401b4000.flexcan: 26
[ 0.771061] flexcan 401b4000.flexcan: 27
[ 0.775148] flexcan 401b4000.flexcan: 28
[ 0.779235] flexcan 401b4000.flexcan: 29
[ 0.783323] flexcan 401b4000.flexcan: )
[ 0.787845] flexcan 401be000.flexcan: device registered (reg_base=(____ptrval____), irq(s):
[ 0.796366] flexcan 401be000.flexcan: 30
[ 0.800454] flexcan 401be000.flexcan: 31
[ 0.804543] flexcan 401be000.flexcan: 32
[ 0.808630] flexcan 401be000.flexcan: 33
[ 0.812717] flexcan 401be000.flexcan: )
[ 0.816921] e100: Intel(R) PRO/100 Network Driver
[ 0.821719] e100: Copyright(c) 1999-2006 Intel Corporation
[ 0.827342] e1000: Intel(R) PRO/1000 Network Driver
[ 0.832315] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 0.838196] e1000e: Intel(R) PRO/1000 Network Driver
[ 0.843257] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 0.849316] igb: Intel(R) Gigabit Ethernet Network Driver
[ 0.854820] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 0.860865] s32cc-dwmac 4033c000.ethernet: IRQ eth_wake_irq not found
[ 0.867438] s32cc-dwmac 4033c000.ethernet: IRQ eth_lpi not found
[ 0.873714] s32cc-dwmac 4033c000.ethernet: no reset control found
[ 0.880045] s32cc-dwmac 4033c000.ethernet: phy mode set to RGMII
[ 0.886268] s32cc-dwmac 4033c000.ethernet: User ID: 0x10, Synopsys ID: 0x52
[ 0.893376] s32cc-dwmac 4033c000.ethernet: DWMAC4/5
[ 0.898443] s32cc-dwmac 4033c000.ethernet: DMA HW capability register supported
[ 0.905897] s32cc-dwmac 4033c000.ethernet: RX Checksum Offload Engine supported
[ 0.913351] s32cc-dwmac 4033c000.ethernet: TX Checksum insertion supported
[ 0.920363] s32cc-dwmac 4033c000.ethernet: Wake-Up On Lan supported
[ 0.926792] s32cc-dwmac 4033c000.ethernet: Enabled workarounds for s32g274a platform
[ 0.934691] s32cc-dwmac 4033c000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 0.942689] s32cc-dwmac 4033c000.ethernet: device MAC address 5e:8a:04:41:3d:72
[ 0.950148] s32cc-dwmac 4033c000.ethernet: Enabled Flow TC (entries=8)
[ 0.956811] s32cc-dwmac 4033c000.ethernet: Enabling HW TC (entries=256, max_off=256)
[ 0.964711] s32cc-dwmac 4033c000.ethernet: Using 32 bits DMA width
[ 0.975406] hwmon hwmon0: temp1_input not attached to any thermal zone
[ 0.983557] hse-uio 40211000.mu1b: firmware not found
[ 0.988862] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 0.995524] ehci-pci: EHCI PCI platform driver
[ 1.000196] usbcore: registered new interface driver uas
[ 1.005641] usbcore: registered new interface driver usb-storage
[ 1.013215] s32gen1-rtc 40060000.rtc: registered as rtc0
[ 1.018655] s32gen1-rtc 40060000.rtc: setting system clock to 1970-01-01T00:00:00 UTC (0)
[ 1.027140] i2c /dev entries driver
[ 1.031067] sac58r-wdt 4010c000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 1.041277] sac58r-wdt 40200000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 1.051473] sac58r-wdt 40204000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 1.061672] sac58r-wdt 40208000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 1.071889] sac58r-wdt 40500000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 1.082086] sac58r-wdt 40504000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 1.092283] sac58r-wdt 40508000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 1.102482] sac58r-wdt 4050c000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 1.112733] sdhci: Secure Digital Host Controller Interface driver
[ 1.119037] sdhci: Copyright(c) Pierre Ossman
[ 1.123479] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.129489] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.129655] mmc0: CQHCI version 5.10
[ 1.136367] hse 40210000.mu0b: firmware not found
[ 1.144662] usbcore: registered new interface driver usbhid
[ 1.150348] usbhid: USB HID core driver
[ 1.165826] s32-adc 401f8000.adc: Device initialized successfully.
[ 1.169538] mmc0: SDHCI controller on 402f0000.mmc [402f0000.mmc] using ADMA
[ 1.183813] s32-adc 402e8000.adc: Device initialized successfully.
[ 1.190307] nxp_s32_ddr_perf 403e0000.ddr-perf: probing device
[ 1.196508] nxp_s32_ddr_perf 403e0000.ddr-perf: device initialized successfully
[ 1.204045] s32-siul2-nvmem 4009c000.nvram: initialize s32 siul2 nvmem driver
[ 1.211442] s32-siul2-nvmem 44010000.nvram: initialize s32 siul2 nvmem driver
[ 1.218915] mmc0: new high speed SDHC card at address aaaa
[ 1.219128] NET: Registered protocol family 10
[ 1.224950] mmcblk0: mmc0:aaaa SC16G 14.8 GiB
[ 1.229762] Segment Routing with IPv6
[ 1.237318] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.238632] mmcblk0: p1 p2
[ 1.243703] NET: Registered protocol family 17
[ 1.250802] can: controller area network core
[ 1.255267] NET: Registered protocol family 29
[ 1.259789] can: raw protocol
[ 1.262809] can: broadcast manager protocol
[ 1.267069] can: netlink gateway - max_hops=1
[ 1.271522] 8021q: 802.1Q VLAN Support v1.8
[ 1.275908] printk: console [ttyLF0]: printing thread started
[ 1.280721] i2c i2c-0: using pinctrl states for GPIO recovery
[ 1.280792] i2c i2c-0: using generic GPIOs for recovery
[ 1.280984] pca953x 0-0022: using AI
[ 1.287840] rtc-pcf85063 0-0051: registered as rtc1
[ 1.287869] i2c i2c-0: IMX I2C adapter registered
[ 1.287910] i2c i2c-0: using dma0chan4 (tx) and dma0chan5 (rx) for DMA transfers
[ 1.288397] i2c i2c-2: using pinctrl states for GPIO recovery
[ 1.288435] i2c i2c-2: using generic GPIOs for recovery
[ 1.288499] i2c i2c-2: IMX I2C adapter registered
[ 1.288534] i2c i2c-2: using dma1chan18 (tx) and dma1chan19 (rx) for DMA transfers
[ 1.288989] i2c i2c-4: using pinctrl states for GPIO recovery
[ 1.289028] i2c i2c-4: using generic GPIOs for recovery
[ 1.289096] i2c i2c-4: IMX I2C adapter registered
[ 1.289124] i2c i2c-4: using dma1chan20 (tx) and dma1chan21 (rx) for DMA transfers
[ 1.289669] phy-s32gen1-serdes 40480000.serdes: Using mode 0 for SerDes subsystem
[ 1.290000] phy-s32gen1-serdes 44180000.serdes: Using mode 3 for SerDes subsystem
[ 1.323422] phy-s32gen1-serdes 44180000.serdes: Unstable RX detected on XPCS1
[ 1.323439] phy-s32gen1-serdes 44180000.serdes: Unstable RX detected on XPCS0
[ 1.323616] s32gen1-pcie 40400000.pcie: Configured as RootComplex
[ 2.324593] s32gen1-pcie 40400000.pcie: Failed to stabilize PHY link
[ 2.324602] s32gen1-pcie 40400000.pcie: Configuring as RootComplex
[ 2.324612] s32gen1-pcie 40400000.pcie: host bridge /soc/pcie@40400000 ranges:
[ 2.324642] s32gen1-pcie 40400000.pcie: IO 0x5ffffe0000..0x5ffffeffff -> 0x0000000000
[ 2.324660] s32gen1-pcie 40400000.pcie: MEM 0x5800000000..0x5ffffdffff -> 0x0000000000
[ 3.321531] s32gen1-pcie 40400000.pcie: Phy link never came up
[ 3.321614] s32gen1-pcie 40400000.pcie: PCI host bridge to bus 0000:00
[ 3.321621] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 3.321629] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 3.321636] pci_bus 0000:00: root bus resource [mem 0x5800000000-0x5ffffdffff] (bus address [0x00000000-0x7fffdffff])
[ 3.321684] pci 0000:00:00.0: [1957:4300] type 01 class 0x060400
[ 3.321726] pci 0000:00:00.0: reg 0x38: [mem 0x5800000000-0x580000ffff pref]
[ 3.321818] pci 0000:00:00.0: supports D1
[ 3.321823] pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold
[ 3.326017] pci 0000:00:00.0: BAR 0: assigned [mem 0x5800000000-0x58000fffff]
[ 3.326028] pci 0000:00:00.0: BAR 6: assigned [mem 0x5800100000-0x580010ffff pref]
[ 3.326037] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 3.326273] pcieport 0000:00:00.0: PME: Signaling with IRQ 82
[ 3.327056] imx_usb 44064000.usb: No over current polarity defined
[ 3.327546] ci_hdrc ci_hdrc.0: EHCI Host Controller
[ 3.327695] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[ 3.345537] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[ 3.345664] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 3.345671] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.345679] usb usb1: Product: EHCI Host Controller
[ 3.345683] usb usb1: Manufacturer: Linux 5.10.120-rt70+g0b76731696c1 ehci_hcd
[ 3.345688] usb usb1: SerialNumber: ci_hdrc.0
[ 3.345989] hub 1-0:1.0: USB hub found
[ 3.346011] hub 1-0:1.0: 1 port detected
[ 3.399221] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 3.399262] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 3.399643] devtmpfs: mounted
[ 3.400133] Freeing unused kernel memory: 1344K
[ 3.505617] Run /sbin/init as init process
[ 3.815713] systemd[1]: System time before build time, advancing clock.
[ 3.864973] systemd[1]: systemd 246 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -ZSTD -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 3.865490] systemd[1]: Detected architecture arm64.

Welcome to Auto Linux BSP 34.0 (gatesgarth)!

[ 3.909037] systemd[1]: Set hostname to <s32g399ardb3>.
[ 3.918286] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.918318] systemd[1]: Initializing machine ID from random generator.
[ OK 4.234468] systemd[1]: Queued start job for default target Multi-User System.
0[ 4.235371] random: systemd: uninitialized urandom read (16 bytes read)
m[ 4.236324] systemd[1]: Created slice system-getty.slice.
] Created slice system-getty.slice.
[ OK ] Created slice sy[ 4.273644] random: systemd: uninitialized urandom read (16 bytes read)
s[ 4.273980] systemd[1]: Created slice system-modprobe.slice.
tem-modprobe.slice.
[ OK ] Created slice sys[ 4.301899] systemd[1]: Created slice system-serial\x2dgetty.slice.
tem-serial\x2dgetty.slice.
[ OK ] Created slice Use[ 4.325858] systemd[1]: Created slice User and Session Slice.
r and Session Slice.
[ OK ] Started Dispatch P[ 4.345765] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
assword …ts to Console Directory Watch.
[ OK ] Started Forward Pas[ 4.369717] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
sword R…uests to Wall Directory Watch.
[ OK ] Reached target Path[ 4.393729] systemd[1]: Reached target Paths.
s.
[ OK ] Reached target Remot[ 4.417633] systemd[1]: Reached target Remote File Systems.
e File Systems.
[ OK ] Reached target Slice[ 4.437624] systemd[1]: Reached target Slices.
s.
[ OK ] Reached target Swap systemd[1]: Reached target Swap.
[0m.
[ OK ] Listening on Sy[ 4.478076] systemd[1]: Listening on Syslog Socket.
slog Socket.
[ OK ] Listening on initc[ 4.501773] systemd[1]: Listening on initctl Compatibility Named Pipe.
tl Compatibility Named Pipe.
[ OK ][ 4.531843] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 4.532173] systemd[1]: Listening on Journal Socket (/dev/log).
Listening on Journal Socket (/dev/log).
[ OK ] Listening on Jour[ 4.561889] systemd[1]: Listening on Journal Socket.
nal Socket.
[ OK ] Listening on Net[ 4.581992] systemd[1]: Listening on Network Service Netlink Socket.
work Service Netlink Socket.
[ OK ] Listening on udev[ 4.605892] systemd[1]: Listening on udev Control Socket.
Control Socket.
[ OK ] Listening on udev[ 4.625829] systemd[1]: Listening on udev Kernel Socket.
Kernel Socket.
[ OK ] Listening on User [ 4.649809] systemd[1]: Listening on User Database Manager Socket.
Database Manager Socket.
Mounting [ 4.675485] systemd[1]: Mounting Huge Pages File System...
Huge Pages File System...
Mounting 4.697905] systemd[1]: Condition check resulted in POSIX Message Queue File System being skipped.
3[ 4.699741] systemd[1]: Mounting Kernel Debug File System...
9mKernel Debug File System...
Starting 4.729822] systemd[1]: Condition check resulted in Kernel Trace File System being skipped.
;[ 4.730120] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.
3[ 4.731802] systemd[1]: Starting Load Kernel Module configfs...
9mLoad Kernel Module configfs...
Starting Load[ 4.775173] systemd[1]: Starting Load Kernel Module drm...
Kernel Module drm...
Starting Loa[ 4.799214] systemd[1]: Starting Load Kernel Module fuse...
d Kernel Module fuse...
Sta[ 4.825785] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
r[ 4.828782] systemd[1]: Starting Journal Service...
ting Journal Service...
Sta[ 4.864709] systemd[1]: Starting Load Kernel Modules...
rting Load Kernel Modules...
[ 4.877837] sja1110: loading out-of-tree module taints kernel.
[ 4.878433] sja1110 spi5.0: probing uc
[ 4.878554] sja1110 spi5.1: probing switch
[ 4.878796] sja1110 spi5.1: Could not get GPIO from device tree
[ 4.878810] sja1110 spi5.1: [sja1110_post_probe_upload_worker] Trying to initialize switch
[ 4.879318] sja1110 spi5.1: Direct firmware load for sja1110_switch.bin failed with error -2
[ 4.879328] sja1110 spi5.1: request_firmware failed with -2
[ 4.879334] sja1110 spi5.0: [sja1110_post_probe_upload_worker] Trying to initialize uC
[ 4.879361] sja1110 spi5.0: Direct firmware load for sja1110_uc.bin failed with error -2
[ 4.879368] sja1110 spi5.0: request_firmware failed with -2
[ 4.919603] systemd[1]: Starting Remount Root and Kernel File Systems...
[ 4.937055] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 4.937089] ext4 filesystem being remounted at / supports timestamps until 2038 (0x7fffffff)
Starting Remount Root and Kernel File Systems...
Starting 4.985825] urandom_read_iter: 32 callbacks suppressed
3[ 4.985840] random: systemd: uninitialized urandom read (16 bytes read)
9[ 4.987657] systemd[1]: Starting Coldplug All udev Devices...
m[ 4.988396] random: systemd-journal: uninitialized urandom read (16 bytes read)
Coldplug All udev Devices...
[ 5.031363] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.033754] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[ OK ] Finished Load Kernel Modules.
[ OK ] Finished Remount Root and Kernel File Systems.
Mounting FUSE Control File System...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
Starting Apply Kernel Variables...
Starting Create System Users...
[ OK ] Mounted FUSE Control File System.
[ OK ] Finished Coldplug All udev Devices.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Create System Users.
Starting Create Static Device Nodes in /dev...
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /tmp...
Mounting /var/volatile...
Starting Rule-based Manage…for Device Events and Files...
[ OK ] Mounted /tmp.
[ OK ] Mounted /var/volatile.
[ OK ] Started Rule-based Manager for Device Events and Files.
Mounting /var/volatile/tmp...
Starting Network Service...
Starting Load/Save Random Seed...
[ OK ] Mounted /var/volatile/tmp.
[ OK ] Reached target Local File Systems.
Starting Rebuild Dynamic Linker Cache...
Starting Create Volatile Files and Directories...
[ 5.782915] pfeng 46000000.pfe: PFEng ethernet driver loading ...
[ 5.782933] pfeng 46000000.pfe: Version: RTM 1.1.0
[ 5.782937] pfeng 46000000.pfe: Driver commit hash: M4_DRIVER_COMMIT_HASH
[ 5.782941] pfeng 46000000.pfe: Multi instance support: disabled (standalone)
[[ 5.782945] pfeng 46000000.pfe: Compiled by: 10.2.0
pfeng 46000000.pfe: Cbus addr 0x46000000 size 0x1000000
[[ 5.782982] pfeng 46000000.pfe: nxp,fw-class-name: s32g_pfe_class.fw
0[ 5.782988] pfeng 46000000.pfe: nxp,fw-util-name: s32g_pfe_util.fw
;[ 5.783034] pfeng 46000000.pfe: irq 'hif0' : 73
32[ 5.783046] pfeng 46000000.pfe: irq 'hif1' : 74
m[ 5.783057] pfeng 46000000.pfe: irq 'hif2' : 75
[ 5.783063] pfeng 46000000.pfe: HIF channels mask: 0x0007
[ 5.783075] pfeng 46000000.pfe: netif name: pfe0
O[ 5.783081] pfeng 46000000.pfe: DT mac addr: 00:01:be:be:ef:11
K[ 5.783088] pfeng 46000000.pfe: netif(pfe0) mode: std
[ 5.783093] pfeng 46000000.pfe: netif(pfe0) EMAC: 0
[ 5.783098] pfeng 46000000.pfe: netif(pfe0) HIFs: count 1 map 01
pfeng 46000000.pfe: EMAC0 interface mode: 4
[[ 5.783287] pfeng 46000000.pfe: PFE port coherency enabled, mask 0x1e
0[ 5.783465] pfeng 46000000.pfe: Clocks: sys=300MHz pe=600MHz
m[ 5.783479] pfeng 46000000.pfe: Interface selected: EMAC0: 0x4 EMAC1: 0xffffffff EMAC2: 0xffffffff
][ 5.784159] pfeng 46000000.pfe: PFE controller reset done
[ 5.784188] pfeng 46000000.pfe: TX clock on EMAC0 for interface sgmii installed
F[ 5.784242] pfeng 46000000.pfe: RX clock on EMAC0 for interface sgmii installed
i[ 5.784370] pfeng 46000000.pfe: assigned reserved memory node pfebufs@34000000
n[ 5.784410] pfeng 46000000.pfe: assigned reserved memory node pfebufs@34080000
i[ 5.784461] pfeng 46000000.pfe: assigned reserved memory node pfebufs@83200000
s[ 5.784482] pfeng 46000000.pfe: assigned reserved memory node pfebufs@835e0000
h[ 5.821373] pfeng 46000000.pfe: Firmware: CLASS s32g_pfe_class.fw [46564 bytes]
e[ 5.821391] pfeng 46000000.pfe: Firmware: UTIL s32g_pfe_util.fw [20332 bytes]
d[ 5.821421] pfeng 46000000.pfe: PFE CBUS p0x46000000 mapped @ v0xffffffc015000000
[ 5.821427] pfeng 46000000.pfe: HW version 0x101
pfeng 46000000.pfe: Silicon S32G3
[[ 5.821441] pfeng 46000000.pfe: Fail-Stop mode disabled
0[ 5.822888] pfeng 46000000.pfe: PFE_ERRORS:Parity instance created
;[ 5.822900] pfeng 46000000.pfe: PFE_ERRORS:Watchdog instance created
1[ 5.822905] pfeng 46000000.pfe: PFE_ERRORS:Bus Error instance created
;[ 5.822911] pfeng 46000000.pfe: PFE_ERRORS:FW Fail Stop instance created
3[ 5.822916] pfeng 46000000.pfe: PFE_ERRORS:Host Fail Stop instance created
9[ 5.822921] pfeng 46000000.pfe: PFE_ERRORS:Fail Stop instance created
m[ 5.822926] pfeng 46000000.pfe: PFE_ERRORS:ECC Err instance created
C[ 5.822936] pfeng 46000000.pfe: BMU1 buffer base: p0xc0000000
r[ 5.823035] pfeng 46000000.pfe: BMU2 buffer base: p0x34000000 (0x80000 bytes)
e[ 5.824316] pfeng 46000000.pfe: register IRQ 77 by name 'PFE BMU IRQ'
a[ 5.824499] pfeng 46000000.pfe: Firmware .elf detected
t[ 5.824506] pfeng 46000000.pfe: Uploading CLASS firmware
e[ 5.824512] pfeng 46000000.pfe: Selected FW loading OPs to load 8 PEs in parallel
[ 5.827710] pfeng 46000000.pfe: BMU_EMPTY_INT (BMU @ p0x(____ptrval____)). Pool ready.
V[ 5.827719] pfeng 46000000.pfe: BMU_EMPTY_INT (BMU @ p0x(____ptrval____)). Pool ready.
o[ 5.843922] pfeng 46000000.pfe: pfe_ct.h file version"92367c0e25f21f49217a9b08168ad2c8"
l[ 5.858525] pfeng 46000000.pfe: [FW VERSION] 1.5.0, Build: Nov 23 2022, 09:48:33 (), ID: 0x31454650
a[ 5.858850] pfeng 46000000.pfe: Uploading UTIL firmware
t[ 5.858856] pfeng 46000000.pfe: Selected FW loading OPs to load 1 PEs in parallel
i[ 5.861286] pfeng 46000000.pfe: pfe_ct.h file version"92367c0e25f21f49217a9b08168ad2c8"
l[ 5.864709] pfeng 46000000.pfe: VLAN ID incorrect or not set. Using default VLAN ID = 0x01.
e[ 5.864717] pfeng 46000000.pfe: VLAN stats size incorrect or not set. Using default VLAN stats size = 20.
[ 5.864797] pfeng 46000000.pfe: Fall-back bridge domain @ 0x20000a34 (class)
F[ 5.864803] pfeng 46000000.pfe: Default bridge domain @ 0x20000a2c (class)
i[ 5.865086] pfeng 46000000.pfe: Routing table created, Hash Table @ p0x34080000, Pool @ p0x34088000 (65536 bytes)
l[ 5.865329] pfeng 46000000.pfe: Feature err051211_workaround: DISABLED
e[ 5.866851] pfeng 46000000.pfe: MDIO bus 0 disabled: Not found in DT
s[ 5.866858] pfeng 46000000.pfe: MDIO bus 1 disabled: No EMAC
[ 5.870129] pfeng 46000000.pfe: HIF0 enabled
a[ 5.870353] pfeng 46000000.pfe: HIF1 enabled
n[ 5.870559] pfeng 46000000.pfe: HIF2 enabled
d[ 5.870565] pfeng 46000000.pfe: HIF3 not configured, skipped
[ 5.871227] pfeng 46000000.pfe pfe0: registered
D[ 5.871248] pfeng 46000000.pfe pfe0: Subscribe to HIF0
i[ 5.871667] pfeng 46000000.pfe pfe0: Enable HIF0
r[ 5.871829] pfeng 46000000.pfe pfe0: setting MAC addr: 00:01:be:be:ef:11
e[ 5.871859] pfeng 46000000.pfe pfe0: PTP HW addend 0x80000000, max_adj configured to 46566128 ppb
c[ 5.871868] pfeng 46000000.pfe: IEEE1588: Input Clock: 200000000Hz, Output: 100000000Hz, Accuracy: 10.0ns
t[ 5.872345] pfeng 46000000.pfe pfe0: Registered PTP HW clock successfully on EMAC0
o[ 6.004189] s32cc-dwmac 4033c000.ethernet eth0: PHY [stmmac-0:01] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL)
r[ 6.021568] s32cc-dwmac 4033c000.ethernet eth0: Enabling Safety Features
i[ 6.021691] s32cc-dwmac 4033c000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
e[ 6.021930] s32cc-dwmac 4033c000.ethernet eth0: registered PTP clock
s[ 6.025441] s32cc-dwmac 4033c000.ethernet eth0: configuring for phy/rgmii-id link mode
8021q: adding VLAN 0 to HW filter on device eth0
[0m.
[ OK ] Started Network Service.
[ OK ] Finished Rebuild Dynamic Linker Cache.
[ 6.365409] urandom_read_iter: 53 callbacks suppressed
[ 6.365426] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.365463] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.365494] random: systemd: uninitialized urandom read (16 bytes read)
Starting Run pending postinsts...
Starting Rebuild Journal Catalog...
Starting Network Name Resolution...
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Finished Update UTMP about System Boot/Shutdown.
[ OK ] Finished Rebuild Journal Catalog.
Starting Update is Completed...
[ OK ] Started Network Name Resolution.
[ OK ] Started Network Time Synchronization.
[ OK ] Finished Update is Completed.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ OK ] Finished Run pending postinsts.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Kernel Logging Service.
[ OK ] Started System Logging Service.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Respond to IPv6 Node Information Queries.
[ OK ] Started Network Router Discovery Daemon.
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
[ 6.897652] random: crng init done
[ 6.897667] random: 54 urandom warning(s) missed due to ratelimiting
Starting User Login Management...
Starting Permit User Sessions...
[ OK ] Finished Load/Save Random Seed.
[ OK ] Finished Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyLF0.
[ OK ] Reached target Login Prompts.
[ OK ] Started User Login Management.
[ OK ] Reached target Multi-User System.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Finished Update UTMP about System Runlevel Changes.

Auto Linux BSP 34.0 s32g399ardb3 ttyLF0

s32g399ardb3 login: root
root@s32g399ardb3:~# ifconfig -a
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

can1 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

eth0 Link encap:Ethernet HWaddr 3A:82:4F:63:4B:77
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:63 Base address:0x6000

lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

pfe0 Link encap:Ethernet HWaddr 00:01:BE:BE:EF:11
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Memory:46000000-46ffffff

sit0 Link encap:IPv6-in-IPv4
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

root@s32g399ardb3:~# ifconfig pfe0 up
[ 39.744179] pfeng 46000000.pfe: HIF0 started
[ 39.744205] pfeng 46000000.pfe pfe0: configuring for fixed/sgmii link mode
[ 39.744607] pfeng 46000000.pfe pfe0: Link is Up - 2.5Gbps/Full - flow control off
[ 39.744831] IPv6: ADDRCONF(NETDEV_CHANGE): pfe0: link becomes ready
root@s32g399ardb3:~# ifconfig pfe0 hw ether 1A:11:77:00:06:01
root@s32g399ard[ 39.792012] pfeng 46000000.pfe pfe0: setting MAC addr: 1a:11:77:00:06:01
b3:~# ifconfig pfe0 192.168.0.1 netmask 255.255.255.0
root@s32g399ardb3:~#

 

标记 (3)
0 项奖励
回复
11 回复数

8,754 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @yellapu_anishkh

chenyin_h_0-1704790588661.png

 

I was using the settings above for the test.

EMAC0 connected to Serdes1-lane0(could be used with P2, P4 by default mapping), EMAC1 connected to Serdes1-lane1(used with P5 by default)

When I tested for PFE0 in kernel/uboot, I used the P2 and P4, in total 3 ports involved, P5 is not related with PFE0, but PFE1.

0 项奖励
回复

8,761 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @yellapu_anishkh

It is my pleasure to support

As is shown in my previous post, I tested PFE_EMAC0 with both port2 and port4.

Port4 is with a 100Base-Tx PHY and is connected to the SJA1110 network switch, while port5 is with a AQR113C PHY and is directly connected to the Serdes-1, the connection and PHY used are different for the two ports.

0 项奖励
回复

8,757 次查看
yellapu_anishkh
Contributor IV

Hi chenyin_h,
We are inline with the above understanding. But our focus is as per your log.
In the log you have shared you tested PFE_MAC0 with SGMII. port5 is with SGMII for PFE_MAC0 on SERDES Lane 1.
But the SERDES config used by you is for Lane 0 as below.
hwconfig=pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=2G5

How this configuration is working for you.

 

0 项奖励
回复

8,771 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @yellapu_anishkh

chenyin_h_0-1704780563259.png

From the BSP user manual, by default, the network ports mapping are shown above, PFE_EMAC1 mapped to the P5 port, not PFE_EMAC0, while the PFE_EMAC0 routed to the SJAxxx and could be used via P2 and P4.

I was using DIP Switches that default to the QSPI boot.

0 项奖励
回复

8,767 次查看
yellapu_anishkh
Contributor IV

Hi @chenyin_h,

Thank you for the response. For your testing of PFE_MAC0, which port is used. port 4 ?
reason is if SGMII is used port 4 (for 2.5G) should be bigger similar to port 5.

0 项奖励
回复

8,788 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @yellapu_anishkh

Good day!

The test we have done are:

  1. PFE0, tested with P2A, P2B, P4 ports, which are all working correct(tested in both uboot and kernel).
  2. PFE1, tested with P5 port, the port pointed out from your attached picture, is working correct also.(Tested in the kernel)
  3. PFE2, tested with P3B port, is working correct.(Tested in the kernel)
0 项奖励
回复

8,777 次查看
yellapu_anishkh
Contributor IV

Hello chenyin_h,

Good Day,

Thank you the response.

We are looking for the same scenario as per your log. PFE0 SGMII, as per the table attached in image "2.png" there is no SGMII on P2A, P2B, P4 ports. Could you please confirm the port used for testing PFE0 SGMII.

Thank You,

0 项奖励
回复

8,806 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @yellapu_anishkh

I feel sorry for your inconvenience, the BSP list is shown correctly from my side following the method provided in the last post, which also include the BSP34.0 images and corresponding documents. Would you please log out, clear the browser cache and then relog in the NXP.com, to further check if it is correct?

we are sorry that due to our service policy, we cannot share the document via this public community, In common, you should see all the available BSP versions for your account. If you don't see the specific version you are looking for, help us contacting your local NXP FAE/representative, for them to start the required process to provide the access.

My testing log is attached for your reference, hope that it could be useful for addressing the issue.

0 项奖励
回复

8,805 次查看
yellapu_anishkh
Contributor IV

Thank you for the log. How is the test performed, have you connected to port 5 or any other port.

Our current testing is with port 5 as shown in attachment.

 

0 项奖励
回复

8,822 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @yellapu_anishkh

Thank you for the question.

For the user manuals of BSP34.0, you may reference the following method:

- Sign in to your NXP account (link to NXP site: Automotive, IoT & Industrial Solutions | NXP Semiconductors)
- Click on "My NXP Account" (top-right) and click on "Software Licensing and Support" under the "Licensing" section within the window it opens.
- This will redirect you to another page. In this new page, select the option "View Accounts" under the "Software accounts" section.
- This will again redirect you to another page. On this page, you should see an "Automotive SW - S32G - Linux BSP (Cortex-A53)" option, click on it.

In there, you should see all the available BSP versions for your account. If you don't see the specific version you are looking for, help us contacting your local NXP FAE/representative, for them to start the required process to provide the access.

I’ve tested PFE0 port on a local RDB3 with BSP34 images, (with hwconfig=pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=2G5) on which no PFE issues found in both u-boot and kernel, would you please reference the commands and settings according the formal BSP34.0 manuals for additional trial?

Feel free to provide any request if still issues found.

0 项奖励
回复

8,815 次查看
yellapu_anishkh
Contributor IV

Hi,

Thank you for the prompt response. Unfortunately the BSP34 document is missing in NXP website.

only available for BSP33 and BSP35.

Could you please share user manual  and log.

0 项奖励
回复