PFE MDC/MDIO PL_01 PL_02 erro

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PFE MDC/MDIO PL_01 PL_02 erro

1,262件の閲覧回数
longfeiwang
Contributor III

Because my design is different from the RDB Design, I use PL_01, PL_02 for the MDC/MDIO control pins of PFE1.

DTS configuration

/* PL01 */
#define PL01_MSCR_S32G        (177)
#define PL01_PFE1_MDC_CFG    (SIUL2_MSCR_S32_G1_MUX_ID_4 | \
    MDC_PIN_CFG)

/* PL02 */
#define PL02_MSCR_S32G        (178)
#define PL02_PFE1_MDIO_CFG    (SIUL2_MSCR_S32_G1_MUX_ID_4 | \
    MDIO_PIN_CFG)
#define PL02_PFE1_MDIO_IN    (SIUL2_MSCR_S32_G1_MUX_ID_3)

 

2)uboot pfe1_mdio configuration in DTS

pinctrl0_pfe1_mdio: pinctrl0_pfe1_mdio {
            fsl,pins = <PL01_MSCR_S32G PL01_PFE1_MDC_CFG
                    PL02_MSCR_S32G PL02_PFE1_MDIO_CFG
                    >;
        };

When my Uboot is started, an error message is generated.

longfeiwang_0-1634868919620.png

 

0 件の賞賛
返信
2 返答(返信)

1,168件の閲覧回数
longfeiwang
Contributor III

The problem has been solved Thank you very much

0 件の賞賛
返信

1,211件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

Hi Longfei,

I can't verify this here but could you find out what the configuration of the GMAC MDIO pins are if the GMAC is still in the device tree?

0 件の賞賛
返信