Hi,
I am working on S32G-VNP-EVB board. i have compiled a sample binary using S32DS3.4 to glow led using rtc example, which runs on M7.
S32G Debug probe:
From S32G Debug probe when connected to target, ELF is working.
Application Bootloader:
Application bootloader is created as a raw binary with below address.
0x3400C000
In Linker file, made below changes as 8MB SRAM is there on EVB.
From u-boot initialized SRAM using below command.
initsram 0x34000000
ext4load mmc 0:2 0x3400c000 /boot/blob.bin
startm7 0x3400c000 //Tried with reset_handler address also//
After this LED is not glowing, which confirms image is not starting.
Clarification: Please provide the correct linker file for EVB.
IVT + DCD + App Binary should be copied to SDCARD and run from SRAM.
Please provide us the correct DCD to be used for this process.
Thanks in advance.