Is the S32G2-VNP-RDB2 board compatible with the auto_yocto_bsp ubuntu image?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the S32G2-VNP-RDB2 board compatible with the auto_yocto_bsp ubuntu image?

520件の閲覧回数
Gerry15
Contributor III

Hello,

 

I already use the auto_yocto_bsp for running the S32G-VNP-RDB2 development board, but I always build the image with the normal -m "non-ubuntu" option. There is also the option to build the image with ubuntu(-base), would this work on this board?  

タグ(3)
0 件の賞賛
4 返答(返信)

505件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Besides it works, we don;t recommend to use the ubuntu mage since all features included in yocto for auto will lost.

Regards

 

0 件の賞賛

492件の閲覧回数
Gerry15
Contributor III

Hey,

thank you for the quick answer. What are the auto features concretely? Further, what is the difference between `fsl-image-ubuntu` `fsl-image-ubuntu-base`? 
P.S. what is the standard login for 'fsl-image-ubuntu'? I could not find any discription from NXP.

Sincerely


Gerry

0 件の賞賛

475件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Since it not from NXP, But the BSP for Auto included drivers like CAN that are not in the ubuntu image, the ubuntu image just include the GUI and network.

Regards

 

0 件の賞賛

401件の閲覧回数
Gerry15
Contributor III

Hey,

 

thank you for the answer. Unfortunately I am still not able to find out the login credentials for the `s32g274ardb2ubuntu` image.

As already discussed here Solved: login username and password failure - NXP Community, I have the right MACHINE activated, which is the s32g274ardb2ubuntu. "root root" does not work.

Do you have the login credentials documented somewhere?

 

Kind regards

 

Gerry

0 件の賞賛