Installed Packages in Gold VIP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installed Packages in Gold VIP

477 Views
akhil_k_appu
Contributor III

hi,

we tried to list the installed packages using the following commands,

apt list --installed

but, it resulted in 

apt: command not found

is there any different way to list the installed packages and components.

0 Kudos
Reply
1 Reply

469 Views
gmocanu
NXP Employee
NXP Employee

Hello,

 

The GoldVIP target image does not include any package management tool by default. The Software-Content-Register (SCR) file that is included in the GoldVIP release would be the best choice to get an overall picture of what packages are included in the image (check the subcomponents list for the "Linux BSP" entry). Note that this is a list with all the packages that are installed in all the domains (both dom0 and v2xdomu), while each VM has a specific set of packages installed.


You can install or remove packages by building a custom image starting from the GoldVIP meta layer (please check the 19th chapter from the GoldVIP User Manual for steps on how to set up the yocto workspace). Also, you will be able to check the list of installed packages by checking the manifest files generated by bitbake (i.e., the content of <yocto_workspace_path>/build_s32g274ardb2/tmp/deploy/images/s32g274ardb2/fsl-image-goldvip-s32g274ardb2.manifest).

 

Best regards,

George

0 Kudos
Reply