Hello,
We are trying to build IPCF_FreeRTOS_S32G399A_M7_0 example in IPCF 4.9.0 using S32DS 3.5.3
We built the bin file and we copied it to the FAT partition of the SD card.
When we try to run the following logs
as per the above steps, the expected output should be like
but we are not getting anything.
We are using S32DS 3.5.3 , IPCF 4.9.0 and RTD 4.0.2 and Linux BSP 38.0.
Please let us know how to proceed.
Hello, @Abhiram_m_s
Thanks for the question.
The package you mentioned is AUTOSAR OS, which is not a public release.
Sorry for your inconvenience.
Best Regards
Chenyin
Hello, @Abhiram_m_s
Thanks for the reply and sorry for the delay
We have the following suggestion for your reference
Seems the RTD version and BSP version are correct, how about the RTOS version used in your examples?
2. You may check the logs by dmesg | grep ipc-shm after executing the commands from your previous post.
3. The default IPCF version under BSP38.0 is IPCF v4.8.0(not IPCF4.9), so that when using the examples with the default settings, it is actually BSP38.0 (with IPCF v4.8.0) + IPCF v4.9.0, Which is causing problems. If you wish to use IPCF 4.9.0, you need to also update the BSP38.0 IPCF version to v4.9.0
Hope it helps
Best Regards
Chenyin
I am not finding the link to download NXP_RTOS_4_4_148_CODEDROP_0_4_0_D2309. Can you please share the link to download this package ?