Hello @chenyin_h ,
It was my fault , i dint change the boot Switch , to load from Nor flash ,
Now I am able to execute the script
Thank you for the support
Regards
Karthik Mallya M
Hello, @Karthik_7
From the logs you provided, the test seems failed, since with a successful test, there should be some logs generated after several seconds when executing the script.
Hope it helps.
Best Regards
Chenyin
Hello @chenyin_h ,
So, could you suggest me any other way to make sure software is functional on M7 core,
Is there any way to debug.?, what do u use for debugging this package?
Regards
Karthik
Hello @chenyin_h and Team ,
I just run a Can-fast-path script by just looping back the Flex can 0 to Flex can 1,just to confirm the A core functionality is fine executing this script i found the below observation .
1. Loop back was successful and able to receive all data .(which was not happening when i tried using FlexCan-0 to LLCE can0 and LLCE can -1 to Flex can1)
2. I understand script will also provide the CPU load of M7-0 and M7-1 which here in this case it is 0
So could you please help me to know why my M7 cores are not running .?and how can i debug this issue?
Thank you
Regards
Karthik
Hello, @Karthik_7
Thanks for the feedback.
Seems there is something wrong with you network from the logs.
A alternative way is to put the SD card on your host, say it is sdh, mount the sdh1 to the host, and copy the goldvip-gateway.bin to sdh1.
Then unmount the SD card, insert it to the board, while under u-boot, reference the following command to load it from the SD card to the ddr:
mmc rescan;
fatload mmc 0:1 ${loadaddr} goldvip-gateway.bin
Then the binary could be loaded the ddr for the following work.
Hope it helps
Best Regards
Chenyin
Hello @chenyin_h ,
It seems like the with above command, provided by you its working you can check the below log.
In order to verify the functionality of the can-gw software, as mentioned in the GoldVIP user manual i tried one of the examples, can slow path the response was as below , i dint understood this behavior
Even to verify the software is running i tried connecting to lauterbach ,but since we do not have a proper CMM script , i was not able to load the symbols, it was throwing bus error for all the atempt .
So could you suggests me, how i can verify, that the M7 core is running smoothly?
Thank you
Karthik
Hello, @Karthik_7
For loading the goldvip-gateway.bin which is newly compiled yourself to your board, from my understanding, both the following ways could be correct.
You may choose any option according to your working environment.
Best Regards
Chenyin
Hello, @Karthik_7
Thanks for your reply and sorry for the delay
For running the can-gw application from the M core, you may reference the following steps:
1. Find the pre-built binaries from GoldVIP, under GoldVIP-S32G3-1.11.0/binaries, use the dd command to flash the image to a SD card
sudo dd if=./fsl-image-goldvip-s32g399ardb3.sdcard of=/dev/sdh status=progress bs=1M && sync
2. Boot the board via SD, under u-boot, use the following commands:
run write_goldvip_images
Then tftp the application file you had built from EB(note: use the .bin file, not the .elf file from the output/bin)
tftp $loadaddr goldvip-gateway.bin
sf erase 0x00400000 +${filesize}; sf write ${loadaddr} 0x00400000 ${filesize};
Then the application you built is successfully flashed to the QSPI flash.
3. Reset the board, the can-gw application could be correctly load and run on M7 core automatically.
For CMM files, there are no CMM files for directly running the elf file in SRAM for this examples, you may have to write it yourselves.
Hope it helps.
Best Regards
Chenyin
Hello @chenyin_h ,
Thank you for the response,
I am trying out steps recommended by you.
I have a concern regarding step 2.
I understood that I need to use goldvip-gateway.bin from the newly built output folder,to load it through tftp.
But before performing step 2 ,do I need to copy goldvip-gateway.bin to the SD card ,
If yes , can I copy it directly or do I need to follow any specific command ,
If no , what is the procedure I need to perform to get it from my output directory.
Thank you,
Regards
Karthik
Hello, @Karthik_7
Thanks for the question.
Now I am verifying it using the same version GoldVIP you shared, once updated, I will share the details ASAP
Besides, I noted that the other thread raised by you is similar to this request, would you mind if I replied from this thread together?
Sorry for your inconvenience.
Best Regards
Chenyin