Hi all,
I'm trying to setup ethernet communication with S32G PFE0 and a Realtek Phy (RTL9010AA) which is connected via RGMII.
PFE Firmware 0.9.4 gets recognized by u-boot and PFE_MAC_0 gets enabled. But during kernel startup there is nothing recognized or configured in pfeng and i dont see pfe adapters with ifconfig.
PFE Firmware is flashed on an eMMC. BSP29 is used.
Is there something specifc to be configured in the kernel? Where can i start to analyze?
Solved! Go to Solution.
There are some steps need to check:
1. Ensure hardware connection is correct.
2. Check pfe0 pinctrl(mii, mdio) and clock configuration in U-boot and Linux device tree.
2. "phy-mode", "phy-handle" and phy address should be set correctly in Linux device tree.
3. "RTL9010AA" driver should be enable via menuconfig.
menuconfig->Device Drivers-> PHY Device support and infrastructure -> Drivers for Realtek PHYs
4. Rebuild the image
5. Boot up the board and set "pfeng_mode" by "setenv pfeng_mode enable,rgmii,none,none"
There are some steps need to check:
1. Ensure hardware connection is correct.
2. Check pfe0 pinctrl(mii, mdio) and clock configuration in U-boot and Linux device tree.
2. "phy-mode", "phy-handle" and phy address should be set correctly in Linux device tree.
3. "RTL9010AA" driver should be enable via menuconfig.
menuconfig->Device Drivers-> PHY Device support and infrastructure -> Drivers for Realtek PHYs
4. Rebuild the image
5. Boot up the board and set "pfeng_mode" by "setenv pfeng_mode enable,rgmii,none,none"