Hi everyone,
I have a question about reference manual,
In S32G2RM it says DDR Subsystem base address is 0x403D_0000
but in attachment of reference manual (S32G2_Memory_Map.xlsx) it says DDR Subsystem base address is 0x4038_0000, which one is correct? and also i could not find register for
解決済! 解決策の投稿を見る。
Hi,
We have received the following update on regards of this topic:
"
By the way, 0x4038_0000 is the start address of DWC_DDRPHYA_ACSM0 register and means the DWC_DDRPHYA_ACSM0 base address.
So, there represents different meaning on the S32G2 RM and S32G2 RM attached.
"
As for the "DDR_PHYA_APBONLY_UCTWRITEONLYSHADOW" register, the following is told:
"...although customer has not the information of DDR_PHYA_APBONLY_UCTWRITEONLYSHADOW, it will also not be impacting the usage."
Please, let us know.
Hi,
Can you let us know from which Reference Manual version you are using? Is the memory map taken from this same Reference Manual version?
Also, we cannot find the register you are mentioning under the S32G2 Reference Manual v7, where are you finding it?
Please, let us know.
these are two inconsistent info taken from RM and RM's attachment excel file,
Hi,
We have received the following update on regards of this topic:
"
By the way, 0x4038_0000 is the start address of DWC_DDRPHYA_ACSM0 register and means the DWC_DDRPHYA_ACSM0 base address.
So, there represents different meaning on the S32G2 RM and S32G2 RM attached.
"
As for the "DDR_PHYA_APBONLY_UCTWRITEONLYSHADOW" register, the following is told:
"...although customer has not the information of DDR_PHYA_APBONLY_UCTWRITEONLYSHADOW, it will also not be impacting the usage."
Please, let us know.
thanks for reply,
I was trying to initialize LPDDR 2GB RAM in custom board and DDR_PHYA_APBONLY_UCTWRITEONLYSHADOW register reading returned 0xFF (means failure) in initialization sequence so i thought to get information about this register in order to understand the fail reason, but after applying initialization code generated by S32DS DDR Tool for 2GB LPDDR according to related RAM parameters, it did not return 0xFF anymore, it fixed now.
best,
Hi,
The revision of the Reference Manual is not the latest one, we always recommend using the latest one.
Still, we have found the inconsistency on the latest revision, thanks for your feedback.
We recommend following the Reference Manual as for the base address, but we will confirm which of the 2 is correct or why the inconsistency.
Please, let us know.