no signal when run lin examples for S32K118EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

no signal when run lin examples for S32K118EVB

588件の閲覧回数
QiujuYe
Contributor III

When use two S32K118EVB boards to run the LIN master and slave examples, there is no signal on LIN bus.

Work environment:  two S32K118EVB boards, one run the lin_master_s32k118 example, another run the lin_slave_s32k118 example, the LIN examples are from S32SDK_S32K1xx_BETA_2.9.0.  The J11-1 is connected with one duport female cable between two boards, then no signal.  

 According to the document S32SDK_S32K118_UserManual.pdf,  lin master and slave examples show 5 dupont female cables are needed, so whether the connection is wrong? if wrong, how to use 5 female cables to connect the two boards?

 

ラベル(1)
3 返答(返信)

499件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

external power supply (12V) must be connected to J16, so board's LIN transceiver is powered. Master node must have jumper J108 placed. Then boards are connected with LIN (J11.1) and GND (J11.4) wires.

BR, Petr 

499件の閲覧回数
QiujuYe
Contributor III

Hi Petr,

Thanks very much for your reply. Now I understand the LIN transceiver can not be powered by USB port. Can you tell me the current value for external power supply(12V) ?

Best Regards

Qiuju.ye

0 件の賞賛

499件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I think you should have at least 500mA power supply.

BR, Petr