S32R41_M7_RTOS_4_7_BETA_0_9_0_DS_updatesite_D2306 is not fully installed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32R41_M7_RTOS_4_7_BETA_0_9_0_DS_updatesite_D2306 is not fully installed

1,023件の閲覧回数
RanDong
Contributor I

1.jpg

The RTOS S32R41 0.9.0 can't installed,How should I do.

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

1,006件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you elaborate closer the issues. Is there any error message or so?

Best regards,

Peter

0 件の賞賛
返信

967件の閲覧回数
RanDong
Contributor I

Hi,

Look at the picture below.1.jpg

0 件の賞賛
返信

933件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

As I understand it the installation is condition by having installed S32R RTD package.

Do you have one installed?

best regards,

Peter

0 件の賞賛
返信

623件の閲覧回数
WenChao
Contributor II

I have already installed RTD, why do I still remind RTD that S32R.root cannot be found

WenChao_0-1701400580239.jpeg

WenChao_1-1701400658313.png

 

0 件の賞賛
返信

904件の閲覧回数
RanDong
Contributor I

 

Hi,

Is there a configuration manual for this component for RTOS_S32R41.

1.jpg

best regards,

Dong.

 

0 件の賞賛
返信

889件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

All manuals should be included in the install package.

However I am not familiar with language you are using, so I cant tell.

Best regards,

Peter

0 件の賞賛
返信

907件の閲覧回数
RanDong
Contributor I
Hi,
I uninstalled version 0.8, and then installed this version still can't install. This version of the source code can be installed, but the configured components are not.
0 件の賞賛
返信