S32K SDK for IAR IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K SDK for IAR IDE

1,822 Views
hansonhe
NXP Employee
NXP Employee

Dear, 

We have S32K SDK for S32DS IDE, whether we have SDK package for IAR IDE? Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,266 Views
robertboys
Contributor IV

Hello

Keil MDK has this SDK installed as part of the S32K-144 Software Pack:  See attachment.

All you need to do is click on the component you want and it is inserted into your project along with any other files needed.

We are working on S32K-148 at this time.

The eval version of MDK can be used to evaluate and use the SDK (for < 32K).

Bob Boys

0 Kudos
Reply

1,266 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

unfortunately, SDK package is for S32 Design Studio only.

Regards,

Martin

0 Kudos
Reply