Hello.
To create IAR SDK project, do I need to install IAR 7.x?
I just installed IAR 8.x at my laptop.
but, if I create S32DS project based on 'IAR 8.x toolchain' there is no selectable SDK list.
if I create 'IAR 7.x- SDK' project, S32DS shows error finding IAR 7.x toolchain. (But, I didn't installed it.)
So, I wonder I must install IAR 7.x to create SDK project at S32DS.
Added with it, is there approximate schedule to support IAR 8.x SDK?
Best Regards,
Mac.