Not able to create S32K118 Project in S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to create S32K118 Project in S32DS

1,503 Views
ambarishhundeka
Contributor III

Hello ,

I have updated the S32DS for S32K118 Patches.  followed the below link for update :

https://community.nxp.com/docs/DOC-340653 

after updating , I just try to create the S32K118 project , but controller is not listed in the S32K1XX.

followed the below steps :

File -> create-> New S32DS project.

Kindly help in this ASAP.

Thanks in Advance.

Regards,

Ambarish

Tags (3)
0 Kudos
Reply
3 Replies

1,100 Views
martin_kovar
NXP Employee
NXP Employee

Hello Ambarish,

please download and install also update 4 and update 5.

Update 4

S32 Design Studio for ARM 2018.R1 - Update 4 available 

Update 5

https://community.nxp.com/docs/DOC-340678 

Regards,

Martin

0 Kudos
Reply

1,100 Views
ambarishhundeka
Contributor III

Hello Martin,

Thank you for the immediate response.

Currently I am using S32DS Version 1.3 , I will update with Update 4 and update 5.

I will check .

Regards,

Ambarish

0 Kudos
Reply

1,100 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

Also good idea is replace old S32DS ARM v1.3 by  S32DS ARM v2018.R1. If I'm correct - the v1.3 is not supporting S32K118 even with updates. 

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=S32-DS-ARM_v2018 

Jiri