Install S32SDK S32K1XX RTM 4.0.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Install S32SDK S32K1XX RTM 4.0.2

3,147 Views
sergiverdaguerelausa
Contributor II

I am trying to install S32SDK S32K1XX RTM 4.0.2 but after install the downloaded exe the IDE doesn't recognise the installation. There are some guide describing the instalation throught .zip file but on downloads only are there the exe.

How to indicate to S32Design Studio to use my already installed S32SDK S32K1XX RTM 4.0.2 ?

 

Thank's!

Sergi

Labels (1)
0 Kudos
Reply
8 Replies

3,125 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @sergiverdaguerelausa 

Which version of S32DS are you using?

This S32 SDK is delivered bundled in the S32 Design Studio v3.4. In this case, it’s already configured and ready to use.

 

B.R.

VaneB

0 Kudos
Reply

2,479 Views
DavidShu
Contributor II

My S32 Design Studio Version is v3.5, and my current S32SDK S32K1XX RTM Version is 4.0.1. how should i get v4.0.2? i could only see v4.0.1 in Design Studio update Center

0 Kudos
Reply

3,090 Views
sergiverdaguerelausa
Contributor II

Hi @VaneB

I am working with S32 Design Studio for S32 Platform 3.4 version.

On S32DS Extensions and Updates there is S32SDK S32K1XX RTM 4.0.3 but I want install 4.0.2.

 

Thank's for answer!

 

Sergi

0 Kudos
Reply

3,079 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @sergiverdaguerelausa 

You should be able to find it at Help -> S32DS Extensions and Updates

VaneB_0-1679940908704.png

 

0 Kudos
Reply

3,065 Views
sergiverdaguerelausa
Contributor II

Hi,

As you can see on the screenshot I don't have 4.0.2, only the last one. 

sergiverdaguerelausa_0-1679986099468.png

Thank's,

0 Kudos
Reply

3,046 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @sergiverdaguerelausa 

Download S32 Design Studio 3.4 S32K1xx Service Pack 1 (SW32K1_S32DS_3.4.1_D2106.zip) at My NXP Account -> Software Licensing and Support -> Software accounts and add it as an updated site.

VaneB_1-1680037506525.png

Please let me know if this works for you.

0 Kudos
Reply

1,720 Views
Eason_L
Contributor III

Hi VaneB,

After installing SW32K1_S32DS_3.4.1_D2106.zip, there's no RTM 4.0.1. How can I get RTM 4.0.1.

Eason_L_0-1701420285423.png

 

0 Kudos
Reply

3,026 Views
sergiverdaguerelausa
Contributor II

Hi @VaneB

It works!

Thank you,

 

Sergi

0 Kudos
Reply