I am trying to install S32SDK S32K1XX RTM 4.0.2 but after install the downloaded exe the IDE doesn't recognise the installation. There are some guide describing the instalation throught .zip file but on downloads only are there the exe.
How to indicate to S32Design Studio to use my already installed S32SDK S32K1XX RTM 4.0.2 ?
Thank's!
Sergi
Which version of S32DS are you using?
This S32 SDK is delivered bundled in the S32 Design Studio v3.4. In this case, it’s already configured and ready to use.
B.R.
VaneB
My S32 Design Studio Version is v3.5, and my current S32SDK S32K1XX RTM Version is 4.0.1. how should i get v4.0.2? i could only see v4.0.1 in Design Studio update Center
Hi @VaneB,
I am working with S32 Design Studio for S32 Platform 3.4 version.
On S32DS Extensions and Updates there is S32SDK S32K1XX RTM 4.0.3 but I want install 4.0.2.
Thank's for answer!
Sergi
Hi,
As you can see on the screenshot I don't have 4.0.2, only the last one.
Thank's,
Download S32 Design Studio 3.4 S32K1xx Service Pack 1 (SW32K1_S32DS_3.4.1_D2106.zip) at My NXP Account -> Software Licensing and Support -> Software accounts and add it as an updated site.
Please let me know if this works for you.
Hi VaneB,
After installing SW32K1_S32DS_3.4.1_D2106.zip, there's no RTM 4.0.1. How can I get RTM 4.0.1.