I installed S32K1_ISELED_RTM_3.0.0 in the directory of S32SDK_S32K1xx_RTM_3.0.0 . Then create the project from Example , and the error report like below:
and the component like below:
What should do ? thanks for any assistance.
PS: Just installed "Hooks for S32DS S32K1xx RTM SDK 3.0.0" and "S32 DS S32K1xx RTM SDK 3.0.0" and "S32 DS S32K1xx RTM SDK 3.0.0 path"
It‘s worked,and thanks for assistance.
Another question: the document say : "after 10000 commands , all ISELED function will return DGIED_EVALUATION_OVER......so digLED_Init_Init_Interface must be called". when I called function digLED_Init_Interface(), it will cast 1 second that the led can not do anything. Is there any other method to reinitialized the solve this problem in shorter time ?