I can't find the components window in the S32K DS v3.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I can't find the components window in the S32K DS v3.5

跳至解决方案
1,206 次查看
Zyuan17
Contributor III

Hi,

I am using S32K DS 3.5 to build my project, and I can't find the components window in the IDE. It appeared once when I first use this software, but the window showed: "due to some problem related to JAVA, the components can't be shown" (I can't remember, but that's what that sentence means). And then I reinstall the software and the components window disappeared. I have checked the window tab, and there is no components option, which means the window is not hiding.

Zyuan17_0-1666483871753.png

 

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,167 次查看
Senlent
NXP TechSupport
NXP TechSupport

Yes, you may see the screenshot, it may be S32 DS V2.2

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,180 次查看
Senlent
NXP TechSupport
NXP TechSupport
0 项奖励
回复
1,173 次查看
Zyuan17
Contributor III
Hi Senlent, instead of an individual window, the S32KDS now move this window to a tab? I have checked some screenshot on the internet and it seems like the S32KDS3.5 still have that window.
0 项奖励
回复
1,168 次查看
Senlent
NXP TechSupport
NXP TechSupport

Yes, you may see the screenshot, it may be S32 DS V2.2

0 项奖励
回复