I can't find the components window in the S32K DS v3.5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I can't find the components window in the S32K DS v3.5

Jump to solution
1,311 Views
Zyuan17
Contributor III

Hi,

I am using S32K DS 3.5 to build my project, and I can't find the components window in the IDE. It appeared once when I first use this software, but the window showed: "due to some problem related to JAVA, the components can't be shown" (I can't remember, but that's what that sentence means). And then I reinstall the software and the components window disappeared. I have checked the window tab, and there is no components option, which means the window is not hiding.

Zyuan17_0-1666483871753.png

 

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,272 Views
Senlent
NXP TechSupport
NXP TechSupport

Yes, you may see the screenshot, it may be S32 DS V2.2

View solution in original post

0 Kudos
Reply
3 Replies
1,285 Views
Senlent
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
1,278 Views
Zyuan17
Contributor III
Hi Senlent, instead of an individual window, the S32KDS now move this window to a tab? I have checked some screenshot on the internet and it seems like the S32KDS3.5 still have that window.
0 Kudos
Reply
1,273 Views
Senlent
NXP TechSupport
NXP TechSupport

Yes, you may see the screenshot, it may be S32 DS V2.2

0 Kudos
Reply