hello,
When I execute the program: apex_downsample_upsample_cv, the program outputs:
Cannot find input image data/common/in_gray_256x256.png.
Other routines that need to open the image are the same result.
The BSP version I am using is VisionSDK_S32V2_RTM_1_3_0_img_yocto
The version of visionSDK I am using is VisionSDK_S32V2_RTM_1_3_0_HF1
The board model I am using is SBC-S32V234.
已解决! 转到解答。
hello,
The data folder path is as follows:
The path in the source code is represented as data/common/in_grey_256x256.png,as shown below:
I copied the data/common/in_grey_256x256.png to the development board, and the same path as the apex_downsample_upsample_cv.elf file.Program execution succeeded.
The test process is as follows:
Thank you very much!!!
hello,
The data folder path is as follows:
The path in the source code is represented as data/common/in_grey_256x256.png,as shown below:
I copied the data/common/in_grey_256x256.png to the development board, and the same path as the apex_downsample_upsample_cv.elf file.Program execution succeeded.
The test process is as follows:
Thank you very much!!!