I use the S32 design studio for ARM R1. I import the example of lptmr_periodic_interrupt_s32k144.
It is running ok in the mode of debug_ram,but it is not ok in the mode of debug_flash. I believe the program reset all the time. Should I set some parameters for debug_flash?
Please help me. Thanks a lot.#
I guess there are two advantages of using debug_ram:
So, if you have enough ram, use (at early debug phase) debug_ram to verify the code.
David
Hi,
debug_flash runs program from flash memory (512kB) , debug_ram runs it from MCU's RAM (64kB). There is no special settings. I tried the example - and for me are working both targets (RAM/Flash) without any issue. You can attach project from your workspace - I'll look at it.
Jiri