l can't open the S32 IDE. "Failed to load the JNI shared library"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

l can't open the S32 IDE. "Failed to load the JNI shared library"

880 次查看
ChenBowen
Contributor II
 

ChenBowen_2-1641885581529.pngChenBowen_3-1641885596806.png

 

 

 

 

 

 

0 项奖励
回复
1 回复

846 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @ChenBowen,

This issue appears to be the result of 32-bit vs 64-bit Java. S32 Design Studio for Power Architecture uses 32-bit Java, which is included in the install. However, you have 64-bit Java installed on your PC as well. For some reason, the S32 Design Studio is being forced to use the 64-bit Java, which it is not designed for and this causes the error you see. 

If possible, you could try to remove the 64-bit Java temporarily and then try to execute S32 Design Studio. If it launches cleanly, then we know this is the cause.

Best Regards,

Mike

0 项奖励
回复