can i rename the exist s32ds project about s32k

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

can i rename the exist s32ds project about s32k

跳至解决方案
3,153 次查看
jinhui_wu
Contributor III

i open a example named "lpspi_transfer".

then i add some components in the project.

so it change to my own project,but the name is still "lpspi_transfer".

i want to change a new name,how can i do it?

标签 (1)
0 项奖励
1 解答
2,341 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

I tried with S32DS 1.3 and it works the same way. If the project is created in S32DS v1.3, choose the project, click rename and insert new project name.

Regards,

Martin

在原帖中查看解决方案

4 回复数
2,341 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

if you use S32 Design Studio v2.0 and project is created in this version of S32DS, choose the project you want to rename, click File and choose rename. Please see the figure below:

pastedImage_1.png

Regards,

Martin

2,341 次查看
jinhui_wu
Contributor III

martin:

   for the V1.3 S32DS,is there some measures can solve the problem?

0 项奖励
2,342 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

I tried with S32DS 1.3 and it works the same way. If the project is created in S32DS v1.3, choose the project, click rename and insert new project name.

Regards,

Martin

2,341 次查看
jinhui_wu
Contributor III

oh,That's amazing.thank you very much.

0 项奖励