can i rename the exist s32ds project about s32k

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can i rename the exist s32ds project about s32k

Jump to solution
2,994 Views
jinhui_wu
Contributor III

i open a example named "lpspi_transfer".

then i add some components in the project.

so it change to my own project,but the name is still "lpspi_transfer".

i want to change a new name,how can i do it?

Labels (1)
0 Kudos
1 Solution
2,182 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

I tried with S32DS 1.3 and it works the same way. If the project is created in S32DS v1.3, choose the project, click rename and insert new project name.

Regards,

Martin

View solution in original post

4 Replies
2,182 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

if you use S32 Design Studio v2.0 and project is created in this version of S32DS, choose the project you want to rename, click File and choose rename. Please see the figure below:

pastedImage_1.png

Regards,

Martin

2,182 Views
jinhui_wu
Contributor III

martin:

   for the V1.3 S32DS,is there some measures can solve the problem?

0 Kudos
2,183 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

I tried with S32DS 1.3 and it works the same way. If the project is created in S32DS v1.3, choose the project, click rename and insert new project name.

Regards,

Martin

2,182 Views
jinhui_wu
Contributor III

oh,That's amazing.thank you very much.

0 Kudos