Hello Sir,
we build below, and fail following, could you help us build success?
Thanks
Michael wu
VisionSDK_S32V2_RTM_1_2_0_HF1/s32v234_sdk/demos/isp/isp_ov10640_default/build-v234ce-gnu-linux-d$ make clean;make allsub
......
./kmem.c:2:21: warning: backslash-newline at end of file
char kmem_srec[] = {\
./kmem.c:3:1: warning: missing terminating " character
"\
^
./kmem.c:3:1: error: missing terminating " character
../../../../../isp/graphs/ov10640_default/src/ov10640_default.c:40:1: error: expected expression before ‘static’
static SEQ_FdmaCfg_t FastDMA;
^~~~~~
../../../../../build/nbuild/helpers.mk:156: recipe for target 'ov10640_default-c.o' failed
make[2]: *** [ov10640_default-c.o] Error 1
make[2]: Leaving directory '/home/michaelwu/VisionSDK_S32V2_RTM_1_2_0_HF1/s32v234_sdk/isp/graphs/ov10640_default/static_ov10640_default/build-v234ce-gnu-linux-d'
../../../../../build/nbuild/sub.mk:73: recipe for target 'allsub' failed
make[1]: *** [allsub] Terminated
make[1]: Leaving directory '/home/michaelwu/VisionSDK_S32V2_RTM_1_2_0_HF1/s32v234_sdk/isp/graphs/ov10640_default/static_ov10640_default/build-v234ce-gnu-linux-d'
../../../../build/nbuild/sub.mk:73: recipe for target 'allsub' failed
make: *** [allsub] Terminated
Solved! Go to Solution.
Hello Sir,
We re-download the package, setup the environment and build them.
We got Success!
Thanks for your kindly support.
Michael Wu
Hello Sir,
We re-download the package, setup the environment and build them.
We got Success!
Thanks for your kindly support.
Michael Wu
Hello Jiri,
We have config the environment same as yours highlight, but still get the same compiler failed.
The picture is our setting. I am sure these paths are existed.
Thanks
Michael Wu
Hi,
I can built this demo without any issue (just by calling make allsub). My OS is ubuntu 16.04LTS. Do you have set correct path to compilers?
Jiri