S32R45_SDHC_RTM_xxx Package Install Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32R45_SDHC_RTM_xxx Package Install Error

ソリューションへジャンプ
1,259件の閲覧回数
fyw
Contributor IV

Hi,

    I install the package "S32R45_SDHC_RTM_1_0_0_D2108_updatesite.zip" via S32Design Studio(Version:3.4) and i got some error:

"Cannot complete the install because one or more required items could not be found.
Software being installed: SDHC_STACK S32R45 1.0.0.202108200413 (com.nxp.SDHC_STACK.S32R45.root.1.0.0.feature.feature.group 1.0.0.202108200413)
Missing requirement: SDHC_STACK S32R45 1.0.0.202108200413 (com.nxp.SDHC_STACK.S32R45.root.1.0.0.feature.feature.group 1.0.0.202108200413) requires 'org.eclipse.equinox.p2.iu; com.nxp.FreeRTOS.S32CC.root.2.0.0.feature.feature.group 0.0.0' but it could not be found"

So how can i install the missing requirements?  Thank you!

0 件の賞賛
1 解決策
1,240件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello fyw,

In the release notes provided in the download site for S32R45_SDHC_RTM_1_0_0_D2108_updatesite.zip, there are some installation instructions:

image.png

Did you install all 3 packages? The errors imply that the FreeRTOS S32R45 RTM 2.0.0 package was not installed.

It is also important to note that you should install the exact version listed in the release notes or you will still receive the error. The version compatibility checker is looking for a specific version. For example, if you were to install the FreeRTOS S32R45 RTM 3.0.0 package instead of the 2.0.0, it would again fail. To overcome this, you should install the 1.0.1 version of the S32R45 SDHC RTM package instead of the 1.0.0, then the FreeRTOS 3.0.0 would be accepted.

Best Regards,

Mike

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
1,241件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello fyw,

In the release notes provided in the download site for S32R45_SDHC_RTM_1_0_0_D2108_updatesite.zip, there are some installation instructions:

image.png

Did you install all 3 packages? The errors imply that the FreeRTOS S32R45 RTM 2.0.0 package was not installed.

It is also important to note that you should install the exact version listed in the release notes or you will still receive the error. The version compatibility checker is looking for a specific version. For example, if you were to install the FreeRTOS S32R45 RTM 3.0.0 package instead of the 2.0.0, it would again fail. To overcome this, you should install the 1.0.1 version of the S32R45 SDHC RTM package instead of the 1.0.0, then the FreeRTOS 3.0.0 would be accepted.

Best Regards,

Mike

0 件の賞賛
1,219件の閲覧回数
fyw
Contributor IV

Thank you! I install Version 1.0.1 and it works. 

1,213件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

- If this post answers your question, please click the "Mark Correct" button. Thank you!

0 件の賞賛