After installing S32 DS, I am getting following message
S32 Design Studio for ARM
no FNP_Act_Installer in java.library.path
Also there are no log files generated.
Seen same error. Is there any solutions for this? Regards.
Hello @whinojo,
S32 Design Studio is developed for and tested to work on Windows and Linux. For Linux, the Ubuntu, Debian, and CentOS are options. To see which versions are supported, please check the release notes document. We cannot guarantee it will work on any OS not listed in the release notes. You are on your own for any issues encountered if you choose to install to anything which is not listed.
Best Regards,
Mike
Hi, I have the software installed in Windows.
Regards.
Hello @whinojo,
Please provide the logs:
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs
"C:\Users\{userid}\workspaceS32DS.ARM.2.2\.metadata\.log"
Best Regards,
Mike
Hi @whinojo,
I checked both log files - thank you for providing them.
It seems something happened to the license after installation and activation. Let's try to solve this by the following method:
Trusted Storage is corrupted and needs to be re-initialized.
Windows host:
-> Delete 'C:\ProgramData\FLEXNet'
This folder may be hidden by default, so then it would be necessary to change Windows Explorer settings to show hidden items.
After this, you should be able to re-activate the existing license on your PC
Best Regards,
Mike
Hello @whinojo,
Please check your S32 Design Studio installation. Specifically check the following file:
s32ds.ini
You need to check it for this line:
If this line is missing or set to the wrong path, then it will produce the error you reported.
If the FNP_Act_Installer.dll file is missing from the ...cll/i86 (or x64) folder, or any of these things are not right, it might make sense to install again. Though the installation log looks good, it's possible something did not install correctly and could be resolved via reinstall.
Please let me know your findings.
Best Regards,
Mike
Installing on wine, I found the same error `no FNP_Act_Installer in java.library.path`
when executing
`C:/NXP/S32DS_ARM_v2.2/eclipse/s32ds.exe`
However,
`C:/NXP/S32DS_ARM_v2.2/eclipse/eclipsec.exe`
launched without error.
Hi, has anyone solved this yet? TIA
I also encounter this problem, have you solved it??