S32 Design Studio for S32K 116/ S32K 118 Controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studio for S32K 116/ S32K 118 Controller

1,645 次查看
kavithakakarla
Contributor II

Hi,

I would like to know if S32 Design Studio Arm Based Supports S32K 116 / S32k118.

I have installed S32 DS from the below link and observed that S32K 116/S32K 118 is not listed in the supported devices.

Please let me know if there is any IDE that supports S32K 116/S32K 118.

Also let me know if SDK is available for S32K 116/ S32K 118.

Regards,

Kavitha

标记 (3)
3 回复数

1,361 次查看
martin_kovar
NXP Employee
NXP Employee

Hello Kavitha,

S32 Design Studio for ARM has not supported  S32K 116/118 yet. Also SDK for these microcontrollers is not available yet.

Regards,

Martin

0 项奖励
回复

1,361 次查看
kavithakakarla
Contributor II

Hi Martin,

Thanks for your reply.

Could you suggest if there are any IDE & Compilers  that support S32K 116/118 Controller.

Regards,

Kavitha

0 项奖励
回复

1,361 次查看
martin_kovar
NXP Employee
NXP Employee

Hello Kavitha,

maybe you could check Keil or IAR IDE. Please see links below.

Keil Embedded Development Tools for Arm, Cortex-M, Cortex-R4, 8051, C166, and 251 processor families... 

IAR Systems 

Regards,

Martin