Hi,
I turn on compiler optimizations in my project, but got some errors while trying to rebuild the code:
Program "gcc" not found in PATH [Discovery Options] page in project properties C/C++ Problem
What can I do to fix this error?
Thank you.
解決済! 解決策の投稿を見る。
I had the same problem and solved it with this method:
Add your gcc path to the end of PATH,
for me is ";C:\NXP\S32DS_Power_v2017.R1\Cross_Tools\powerpc-eabivle-4_9\bin"
Done.
I had the same problem and solved it with this method:
Add your gcc path to the end of PATH,
for me is ";C:\NXP\S32DS_Power_v2017.R1\Cross_Tools\powerpc-eabivle-4_9\bin"
Done.
Hi,Jiri jiri.kral@nxp.com
The attachment is the lib_mem.args file.
and I try to use 2017.R1 version to build,but the gcc error also exists.
Thanks
Hi Alex,
the .args file looks okay. So - last chance - can you please share your project or lib_mem library project?
Jiri
Hi,
please check if you have set the prefix for gcc:
and VLE_TOOLCHAIN_DIR/bin points points to folder with cross tools binaries. Also check if the binaries are physically present on the hard drive.
Jiri
Hi, Jiri
I have checked the settings you mentioned above,but they don't work.
I find If I delete the optimization info in .cproject file and then built,the Program "gcc" not found in PATH error message will be removed,but the optimization level of lib_mem.c will be changed from O3(what optimization level I want) to none automatically.
BR
Alex
Hi Alex,
I tried reproduce the issue - but no success. Can you please share the .args file for your lib_mem project with Level 3 optimization enabled?
Are you able use the current S32DS Power version - v2017.R1?
Jiri
Hi,
what is your S32DS version and target MCU?
Jiri
Hello,Jiri
S32DS version :S32 Design Studio for Power Architecture v1.2
Target MCU:S32R274
Thanks.