Problem with S32 Design Studio for Power v1.2 - Update 2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem with S32 Design Studio for Power v1.2 - Update 2

跳至解决方案
1,949 次查看
jobu
Contributor II

Hello,

I get some error messages if I try to install the update. Please see attached file.

Some hints to fix the problem are welcome...

Regards

Jörg

标签 (1)
0 项奖励
1 解答
1,750 次查看
jobu
Contributor II

... I finally manged the update. I have disabled all URLs in "Available Software Sites" and then it works.

Jörg

在原帖中查看解决方案

0 项奖励
3 回复数
1,751 次查看
jobu
Contributor II

... I finally manged the update. I have disabled all URLs in "Available Software Sites" and then it works.

Jörg

0 项奖励
1,751 次查看
jobu
Contributor II

... I have switched off the firewall but no difference. Also my network connection is fine.

Other suggestions?

Jörg

0 项奖励
1,751 次查看
jiri_kral
NXP Employee
NXP Employee

Hello Jörg, 

I updated S32DS right now and have no issue with that. In your case it may be some temporary network outage or firewall issue on your network. If the errors are still present - check the firewall settings and network connection. 

Jiri 

0 项奖励