PEMicro not shown in "Run configuraiton..."

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PEMicro not shown in "Run configuraiton..."

ソリューションへジャンプ
619件の閲覧回数
LeoZ
Contributor III

In S32 Design Studio, "PEMicro" only show in "Debug Configurations" but not show in "Run Configurations"

How could I add "PEMicro" to "Run Configurations". Because I often just want to download code to board to run with the "Run" button, not need to debug

noe_1.jpg

ラベル(1)
0 件の賞賛
返信
1 解決策
604件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

for embedded systems there is no reason for using Run configurations. You always need to use debug probe (except the systems with OS which can execute gdb server). Please use Debug Configurations.  

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
605件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

for embedded systems there is no reason for using Run configurations. You always need to use debug probe (except the systems with OS which can execute gdb server). Please use Debug Configurations.  

0 件の賞賛
返信
585件の閲覧回数
LeoZ
Contributor III

Got it,and I am going to use debug. Actually, I use the "Run" to work as a "download" button for programming code to board without "debug" (no "download" button in S32 Design Studio).

0 件の賞賛
返信