Hi,
In S32 Design Studio for ARM there was a window which showed a Components folder related to the configured components in the Processor Expert.
As I have noticed, the Processor Expert ist now replaced by a new Config Tool. However I miss the very useful components folder, which showed me all the configured components and their related functions. I could even drag and drop the functions straight into code.
Is there anything simular in the 3.5 or do I have to know and type in all functions manually?
Hi @affoltep
Unfortunately, S32DS 3.5 does not have this same functionality, but it has something similar named "Outline view". This view displays an outline of a structured C/C++ file that is currently open in the editor area, by listing the structural elements.
The table below lists the icons displayed and an example using the library "Siul2_Port_Ip.h" (S32K3 devices library).
B.R.
VaneB