A bare metal example project enabling peripheral interrupt (eg. PIT) generated on S32DS for ARM v 1.3 does not work on S32DS for Arm v 2.0 and S32DS for Arm 2018.R1. AjeshKumar
解決済! 解決策の投稿を見る。
Hi Ankur,
I'd suggest you to update vector file (vt_MAC57D54H_M4.s):
.section .vt,"a" /* place vectors into .vt linker section */
vt:
.word _stack_e /* initial SP */
.word exception_trap /* Reset */
/* exceptions*/
.word exception_trap /* 2 NMI */
.word exception_trap /* 3 HardFault */
...
.section .text /* exception_traps, interrupt_trap goes into .text */
.thumb
exception_trap:
b exception_trap
interrupt_trap:
b interrupt_trap
now adjust the linker file:
SECTIONS
{
/* Interrupt vectors area */
.intvec :
{
M4_0_VECTOR_TABLE = .;
M4_0_VECTOR_RAM = .;
KEEP(*(.vt*)) /* avoid removing the section if vt is not referenced */
M4_0_VECTOR_SIZE = .;
} > GRAM
In the .map file you should see now vector table placed at address 0x3F000100:
.intvec 0x3f000100 0x200
0x3f000100 M4_0_VECTOR_TABLE = .
0x3f000100 M4_0_VECTOR_RAM = .
*(.vt*)
.vt 0x3f000100 0x200 ./Project_Settings/Startup_Code/vt_MAC57D54H_M4.o
0x3f000100 vt
0x3f000300 M4_0_VECTOR_SIZE = .
Hope it helps.
Stan
Hi Ankur,
Could you possibly send us the project you are trying to open in a newer S32DS version?
This will help us to resolve this issue much faster.
Thanks!
Stan
Hi Stanislav,
Attached is the project with which I am experiencing the issue. When the project is build/debug through S32DS ver 2.0 I see repeated resets on the hardware and this is always the case. When the same project is build/debug through S32DS ver 1.3 all works well. I will wait for your response.
Regards,
Ankur
Hi Ankur,
I'd suggest you to update vector file (vt_MAC57D54H_M4.s):
.section .vt,"a" /* place vectors into .vt linker section */
vt:
.word _stack_e /* initial SP */
.word exception_trap /* Reset */
/* exceptions*/
.word exception_trap /* 2 NMI */
.word exception_trap /* 3 HardFault */
...
.section .text /* exception_traps, interrupt_trap goes into .text */
.thumb
exception_trap:
b exception_trap
interrupt_trap:
b interrupt_trap
now adjust the linker file:
SECTIONS
{
/* Interrupt vectors area */
.intvec :
{
M4_0_VECTOR_TABLE = .;
M4_0_VECTOR_RAM = .;
KEEP(*(.vt*)) /* avoid removing the section if vt is not referenced */
M4_0_VECTOR_SIZE = .;
} > GRAM
In the .map file you should see now vector table placed at address 0x3F000100:
.intvec 0x3f000100 0x200
0x3f000100 M4_0_VECTOR_TABLE = .
0x3f000100 M4_0_VECTOR_RAM = .
*(.vt*)
.vt 0x3f000100 0x200 ./Project_Settings/Startup_Code/vt_MAC57D54H_M4.o
0x3f000100 vt
0x3f000300 M4_0_VECTOR_SIZE = .
Hope it helps.
Stan
Thanks Stanislav. However I would have liked to see this as by default integrated in the IDE. Under present circumstances, it makes difficult for users to work on interrupts.
Regards,
Ankur
Ankur,
Thanks for the feedback,
let me log this issue into our defect tracking database.
Stan