These problem occurred suddenly,and it's show"Loading com.frescale processorexpert.core",I tried to uninstall it,and install it again,but it no effect.How can I solve this problem.
thank you all.
Thank you all,I have solve this problem.I tried change my work directory,and it works.
Excuse me, how did you change your work directory?
I just rename the directories of my workspaces and now works. Thanks for the suggestion!
Hi,
Which version of S32 Design Studio are you using?
Could you possibly attach log file located in your workspace:
"<your workspace directory>\.metadata\.log"
This will help us to identify the root cause of this issue.
Thanks,
Stan
HI Stanislav,
This problem hasn't solve ,I tried to start this software in Windows Safety Mode ,it still doesn't work.The message is shown above.Please help me to find out the problem.
Hi Stanislaw,
I have the same problem like it is described in the topic. I can not launch the s32 design studio while it is loading the processorexper.core module.
Here are my .log infos:
!SESSION 2018-05-22 08:14:08.548 -----------------------------------------------
eclipse.buildId=4.6.3.M20170301-0400
java.version=1.8.0_51
java.vendor=Oracle Corporation
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=de_DE
Framework arguments: -product com.nxp.s32ds.arm.ide.product
Command-line arguments: -os win32 -ws win32 -arch x86 -product com.nxp.s32ds.arm.ide.product
!ENTRY org.eclipse.cdt.dsf.gdb 4 5012 2018-05-22 16:10:37.022
!MESSAGE Error with command: gdb --version
!STACK 0
java.io.IOException: Cannot run program "gdb": Launching failed
Thanks for help.
HI,
Thank you,Stan.
My software version is S32DS.Version.2.0 ,and I just check the log file,it has stopped record after this issue occurred.The abstract of the log file shows as below.
!SESSION 2018-03-19 16:21:29.517 -----------------------------------------------
eclipse.buildId=4.6.2.M20161124-1400
java.version=1.8.0_51
java.vendor=Oracle Corporation
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=zh_CN
Framework arguments: -product com.nxp.s32ds.vision.ide.product
Command-line arguments: -os win32 -ws win32 -arch x86 -product com.nxp.s32ds.vision.ide.product
!ENTRY org.eclipse.egit.ui 2 0 2018-03-19 16:21:52.590
!MESSAGE Warning: The environment variable HOME is not set. The following directory will be used to store the Git
user global configuration and to define the default location to store repositories: 'C:\Users\juju'. If this is
not correct please set the HOME environment variable and restart Eclipse. Otherwise Git for Windows and
EGit might behave differently since they see different configuration options.
This warning can be switched off on the Team > Git > Confirmations and Warnings preference page.
Thanks.