I can not find my .elf & .map

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I can not find my .elf & .map

ソリューションへジャンプ
1,598件の閲覧回数
tim_wu
Contributor I

Hello everyone, I used S32 DS to development the MPC5744P EV kit, when i created a new project from sample code(Hello world),then I  build the project is normal, but I wanted to debug the project, it seems like a error occured, I check my project document, and I check the problem, the root cause is the debug can not find the .elf & .map file, could you please give me some suggestions or tell me how to solve this problem, really thank you...><

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
1,415件の閲覧回数
tim_wu
Contributor I

Hello, I think the reason is that I delete some files(For example: example project...) in my work space, so I try to uninstall the S32DS last night, then re-install S32DS again,and  the problem  can be solved....haha!

BTW, after I re-install the S32DS,  I feel much faster when I go into the debug mode(120 seconds → 10 seconds).....

I remember the original error message is show "in my workspace path....can not find the elf file", after all, the problem has been solved! 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,415件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share output from your build console? By default the .elf and .map file is in Debug or Debug_FLASH folder. If .elf is not generated - in build console should be shown error message. 

Jiri 

0 件の賞賛
返信
1,416件の閲覧回数
tim_wu
Contributor I

Hello, I think the reason is that I delete some files(For example: example project...) in my work space, so I try to uninstall the S32DS last night, then re-install S32DS again,and  the problem  can be solved....haha!

BTW, after I re-install the S32DS,  I feel much faster when I go into the debug mode(120 seconds → 10 seconds).....

I remember the original error message is show "in my workspace path....can not find the elf file", after all, the problem has been solved! 

0 件の賞賛
返信