Hi,
I want to install ARM V2.2 and 2018R1 on a PC, when I finished install and offline activation, the two IDE can work well , but when I restart the PC, ARM V2.2 IDE will missing License, how to solve it ? thanks !
HI donghua chen
I have installded both versions and work fine
When you installe the second version of the IDE ,you only need to activate it once more
Hello donghua.chen@avnet.com,
Apologies for the long delay in reply.
I assume you will enter the activation code again when this occurs. Does this happen each time you reboot? Is it always S32DS for ARM v2.2 that loses it's license or is it sometimes 2018.R1? It appears to be part of an issue with the trusted storage.
You could try to perform this step, though you would need to activate again after:
-> Delete 'C:\ProgramData\FLEXNet'
This folder may be hidden by default, so then it would be necessary to change Windows Explorer settings to show hidden items.
Then activate v2.2 first and see if problem is solved for both v2.2 and 2018.R1.
Please let us know the result or if the issue is already solved.
Best Regards,
Mike