Hello,
I'm using a development board S32K146 and working with the LPUART, i did the configuration using the SDK 8.5.
The configuration is:
Baud rate: settled as 256000 (no option to set it as 921600)
Parity: no parity
Stop bits: 1
Data: 8 bits
8 bit data + 1 stop bits + start bit
I've change the pins to LPUART0
Tx -> PTB1 output
Rx -> PTB0 input
I configured the FIRCDIV2_CLK at 48MHz as input clk
Using the code example lpuart_echo_s32k146, to get the desired baud rate I write before the initialization of the instance:
lpuart0_InitConfig0.baudRate = 921600U;
Tx communication is successful, frames are written correctly, but when I send the "Hello Board \r\n" string, I don't have the response back.
If I just low the baud rate to the fastest in the SDK the code works as expected...
Any suggestions?