GTM_CFG_Tool License request

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GTM_CFG_Tool License request

2,088 Views
lihui1
Contributor II

There's no email address can get trial license code.

Software send email automatic , the email address is not nxp but freescale  and it's returned by reason "Can not connect to recipiet's server because of unstable network or firewall filter" 

So is there any way could I get the trial license? Thank you!

image001(07-20-17-43-45).jpg

image005(07-20-17-43-45).jpg

0 Kudos
Reply
7 Replies

1,203 Views
GTM
Contributor I

GTM_CFG_Tool License request

0 Kudos
Reply

2,054 Views
mikedoidge
NXP Employee
NXP Employee

Hello @lihui1,

Please place the attached license file (license.txt) into the directory labeled "GTM Configuration Tool\lic" and rename it to license.lic.  This should complete the required installation setup and you should now be fully functional.  If you require further assistance or you have comments or questions please feel free to contact us as you desire.

Best Regards,

Mike

0 Kudos
Reply

2,036 Views
lihui1
Contributor II

Dear Mike:

there's an error , it prompt that system data has been set back. 

The system data cannot be setting because there has a software locked it on our customor's system.

Is there any solution can be solve? 

dbefd008-13b6-414a-a75a-8019d991c668.png

0 Kudos
Reply

2,028 Views
mikedoidge
NXP Employee
NXP Employee

Hello @lihui1,

This error message is from the FlexLM license management software. It is indicating that the time/date of the host machine operating system was modified. This is intended to prevent users of a FlexLM licenses application from extending the usage of the application past the license expiration by changing the system time/date of the OS to a time/date in the past. I think there is no way to disable this security feature. Is there some other host PC which could be used? I could provide a new license for a different PC.

Best Regards,

Mike

0 Kudos
Reply

2,077 Views
mikedoidge
NXP Employee
NXP Employee

Hello @lihui1,

Please attach the request to this thread and we can generate a license for you. The license will be node-locked, so we require the details contained within the generated request form.

Best Regards,

Mike

0 Kudos
Reply

1,997 Views
GTM
Contributor I

Hello .@mikedoidge,

I have exactly the error.

Could you please help me?

Best Regards,

Jay

0 Kudos
Reply

2,069 Views
lihui1
Contributor II

Dear Mike:

Registrants Name: liam
Company Name: lincontrol
Street Address: qingshui
City: wuhan
State/Province: hubei
Zip/Postal Code: 430000
Country: china
Email Address: liuliangming@lincontrol.com


License Information

Host ID: c5f839e
Platform: Windows 8-6.2
License Type: Demo_MPC5746M
License Request Type: Trial

FYI!  Thank you!

0 Kudos
Reply