Hi,
We are using S32 Design Studio.
S32 Design Studio for Power Architecture
Version: 1.2
Build id: 170613
(c) Copyright Freescale Semiconductor 2016. All rights reserved.
(c) Copyright NXP 2017.
Visit http://www.nxp.com/
MCU == MPC5777C
evb == MPC5777C EVB
debugger == Multilink universal fx
Operating System == Win7x64,Win8x64 Till now we were using only Core 0. We have successfully able to debug & test GPIO,PWM,CAN,SPI etc modules using Core 0.
Now we have written pin toggling program in Core 1 & trying to debug it.
It shows that debug done 100%.
But when we try to do single stepping we are not able to do that.
We are setting debug configuration similar to what we are doing for Core 0.
We have stuck here.
Please guide us.
Thanks.
Rahul
Hi,
We tried with the suggested steps.
But we are getting error.
"Error in services launch sequence"
Please guide.
Thanks.
Rahul
Hi,
Following is the details of error.
Following immage shows the server settings in current project.
Please suggest mistakes.
Thanks.
Rahul.
Hi,
you are probably starting second instance of gdbserver by Z7_1 debug. Please check if Z7_1 debug isn't starting gdbserver (screenshot is taken from S32R274 - but it is very similar as your MCU).
and also Z7_1 is only attaching to running server:
Jiri
Hi,
we are able to debug core1.
Thanks.
Rahul.