Error in services launch sequence. PEmicro GDB Launch Failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in services launch sequence. PEmicro GDB Launch Failure

ソリューションへジャンプ
21,732件の閲覧回数
myna
Contributor III

Hello.

When downloading s32k118EBV sample code, the following error occurs.

Error in services launch sequence
PEmicro GDB Launch Failure : Could not bind socket. Address and port are already in use. Another GDB Server debug session may be using the same Server Port number. To run simultaneous debug sessions, please specify a unique Server Port and GDBMI Port in the Debug Configuration for each project. If another session is not running simultaneously, make sure that the chosen port is available and that pegdbserver_console and the arm-none-eabi-gdb processes have terminated.

Please check attached capture file.

How can I solve this problem???

ラベル(1)
1 解決策
21,161件の閲覧回数
myna
Contributor III

I did check netstat, it was already using the gdb port elsewhere.

So, I did change GDB Server port Number in Debug Configuration--> GDB Server Settings

Eventually, the problem was solved.

Thank you.

myna

元の投稿で解決策を見る

5 返答(返信)
21,161件の閲覧回数
myna
Contributor III

I've already checked, but there is no running  pegdbserver_console.

Is there any other solution?

0 件の賞賛
返信
21,162件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

You can check if any other application isn't using gdb server's port. You can use windows commandline> netstat -a -b 

pastedImage_1.png

Assuming that restart of your PC machine also doesn't help, correct? 

Jiri 

0 件の賞賛
返信
21,162件の閲覧回数
myna
Contributor III

I did check netstat, it was already using the gdb port elsewhere.

So, I did change GDB Server port Number in Debug Configuration--> GDB Server Settings

Eventually, the problem was solved.

Thank you.

myna

17,482件の閲覧回数
yangjinzhuang
Contributor IV

What GDB server port number should I set for the two cores?

0 件の賞賛
返信
21,161件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

check if there is no another pegdbserver_console instance running in Windows task manager (CTRL+SHIFT+ESC). If yes - end the task. 

Jiri

0 件の賞賛
返信