Hi,
I was seeking if it is possible to extract code metrics for individual files for the MPC5777C C code. I have come across the utility "NXP\S32DS_Power_v2017.R1\Cross_Tools\powerpc-eabivle-4_9\bin\ powerpc-eabivle-size.exe" which provides the details as below:
text | data | bss | dec | hex | filename |
6036 | 40 | 1120 | 7196 | 1c1c | my_exe.elf |
Is there a utility that can provide code metrics for individual source files?
Regards,
Harsha
解決済! 解決策の投稿を見る。
yes, see Listing Code and Data Size for each Source File with GNU and Eclipse | MCU on Eclipse
I hope this helps,
Erich
yes, see Listing Code and Data Size for each Source File with GNU and Eclipse | MCU on Eclipse
I hope this helps,
Erich
Thanks BlackNight, I would go through the link more thoroughly. Just wanted to know if the information available in the link also works for the S32 design studio IDE for PowerPC architecture.
Thanks,
Harsha
Yes, this is for the GNU tools, so applicable to anything using GNU tools, including the S32 DS.