Mailbox is :
'Launching lpuart_echo_s32k146_debug_flash_pemicro'has encountered a problem.
Could not determine GDB version after sending:D:\software\NXP\S32DS_ARM_v2.2\eclipse\../S32DS/build_tools/gcc_v6.3/gcc-6.3-arm32-eabi/bin/arm-none-eabi-gdb --version,response:
---------------------------------------------------------------------------------------------
Can't Debug S32k Board while I connecting Network
How can I deal with this problem?
when I disconnect the internet,I can debug my s32k board.~
but sometimes I need to connect my PC from remote PC to Debug my remote board.
So I need to deal with this problem......
Wait your reply ,Ths!.
解決済! 解決策の投稿を見る。
Hi,
it must be some netwrork/firewall/port settings (port used for debug may be taken by other application) issue on your PC. If it is your private PC - try to figure out, if the machine is from your company - ask your IT department for fix. You can also try to change port settings in debug configurations:
To be honest - as far I remember - it is very first time when such issue is reported.
Jiri
Hi,
it must be some netwrork/firewall/port settings (port used for debug may be taken by other application) issue on your PC. If it is your private PC - try to figure out, if the machine is from your company - ask your IT department for fix. You can also try to change port settings in debug configurations:
To be honest - as far I remember - it is very first time when such issue is reported.
Jiri
Hi jiri,
Ths for your reply.
I have two company PC also have this issue,and my colleague also have this problem..it may be company IT department do something wrong..but my company IT department they dont't know how to fix it........
I try to change port settings in debug configuration ,but it not work,Can you share what the value should be set in bebug configurations or remote to control my PC to check this issue?
Best Regards , Ths.